EAGLE User Support (English) Prevent PLANE with STOP?
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
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 180 subscribers
  • Views 400 views
  • Users 0 members are here
Related

Prevent PLANE with STOP?

Former Member
Former Member over 11 years ago

Hello,

 

I'm a 1st-time Eagle 6.5 user...

 

I'm using a 0603 package and want to edit it so that my PLANE does not enter a specific area of the package. I drew the area that I don't want the (top) PLANE to go and assigned tSTOP to this area, resaved the package, and it updated on the BRD (I see my newly drawn area... however, the PLANE still is filling in this area.

 

What layer should I assign the specific area to in order to prevent the PLANE from going there?

 

Thank you!

-chuck

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    Sort-of experimented with this and it appears that tRestrict performs this function... anything else I should know?

     

    -chuck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    On 27/03/14 20:46, Chuck Van Dien wrote:

    Sort-of experimented with this and it appears that tRestrict performs

    this function... anything else I should know?

     

    This is all in the manual...

     

    xPlace     Silk screen

    xStop      Solder mask (negative image)

    xCream     Solder paste

    xKeepout   Restricted area for components

    xRestrict  Restricted area for tracks & vias

     

    Try "help layer" for the full list

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    On 27/03/14 20:46, Chuck Van Dien wrote:

    Sort-of experimented with this and it appears that tRestrict performs

    this function... anything else I should know?

     

    This is all in the manual...

     

    xPlace     Silk screen

    xStop      Solder mask (negative image)

    xCream     Solder paste

    xKeepout   Restricted area for components

    xRestrict  Restricted area for tracks & vias

     

    Try "help layer" for the full list

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    This is very helpful, thank you.

     

    I'm using the eval version... I used Eagle CAD ~15 years ago for a small project and swore I would never use it agian being very frustrated (at that time) with creating any custom parts using the library, HOWEVER, decided to try it agian and am finding it to be MUCH MUCH more user-friendly and this forum is AWESOME!

     

    Thank you for everyones help!

    -chuck