EAGLE User Support (English) How can I change the units in the wire width field?
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
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 179 subscribers
  • Views 484 views
  • Users 0 members are here
  • properties
  • units
Related

How can I change the units in the wire width field?

Former Member
Former Member over 11 years ago

The wire (track) width is currently shown in inches. How can I change this to mils? BTW: is there a place where I can view and/or change board properties?

 

Regards,

Stefaan Claes

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    Il 31/03/2014 20:06, Stefaan Claes ha scritto:

     

    The wire (track) width is currently shown in inches. How can I change

    this to mils?

     

     

    grid mil

     

     

    Marco

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Thanks a lot for your quick reply. :-)

     

    The command 'grid mil' changed the units in the wire width field. I find it a bit strange... :-/

    I didn't expect this because I'm not changing the grid.

     

    Regards,

    Stefaan Claes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    Il 31/03/2014 23:50, Stefaan Claes ha scritto:

     

    The command 'grid mil' changed the units in the wire width field. I find

    it a bit strange... image

    I didn't expect this because I'm not changing the grid.

     

     

    From the help:

     

    The GRID command is used to specify the grid and the current unit

     

     

    Best regards!

    Marco

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    Stefaan Claes wrote:

     

    The wire (track) width is currently shown in inches. How can I change

    this to mils?

     

    the GRID command is used to change the unit setting for the whole UI.

    This avoids confusion with diffent units in different places.

     

    If you sometimes want to use a differing unit you can add the unit

    after the value in the input field or command line.

     

     

    BTW: is there a place where I can view and/or change board

    properties?

     

    what board properties? Dimensions, thickness, layer stack, ...?

    --

     

    Lorenz