EAGLE User Support (English) UL_CIRCLE x, y and radius
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
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 180 subscribers
  • Views 413 views
  • Users 0 members are here
Related

UL_CIRCLE x, y and radius

Former Member
Former Member over 11 years ago

Hi All,

 

I'm not sure if this has been answered before, but I've searched for a while and can't find information on it.

 

Is there a way to get the x, y and radius of a circle, including the decimal places, using UL_CIRCLE? When the values are rounded to the nearest integer, it isn't accurate enough for my drawing commands that follow.

 

Thanks for any help in advance.

  • Sign in to reply
  • Cancel
Parents
  • AnalogNotes
    0 AnalogNotes over 11 years ago

    Sorry for the silly question, but why are you rounding to the nearest integer?  Instead of using %d in a sprintf, use %f and you should get the decimal places...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to AnalogNotes

    No problem :-) I'm not rounding to the nearest integer, the UL_CIRCLE command extracts the information as integers from the start:

     

    EAGLE Help: UL_CIRCLE

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • AnalogNotes
    0 AnalogNotes over 11 years ago in reply to Former Member

    Ah, that's a different version of the help than I have.  Which version of EAGLE are you using?  The values in UL_CIRCLE are in the "internal units" of EAGLE and need to be converted to whatever you're comfortable with (mm, mil, etc) using functions like u2mm or u2mil.  See:  EAGLE Help Version 6.5.0 - UL_CIRCLE

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • AnalogNotes
    0 AnalogNotes over 11 years ago in reply to Former Member

    Ah, that's a different version of the help than I have.  Which version of EAGLE are you using?  The values in UL_CIRCLE are in the "internal units" of EAGLE and need to be converted to whatever you're comfortable with (mm, mil, etc) using functions like u2mm or u2mil.  See:  EAGLE Help Version 6.5.0 - UL_CIRCLE

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to AnalogNotes

    Ah, thank you very much. Just upgraded to 6.5 recently and I was working with the old EAGLE help.

     

    It's working perfectly now :-)