Is there a script or something that can format all the component names and values on my board so it's the same size? I tried a group select with the Info tool, but that didn't work. Only one item was changed.
Is there a script or something that can format all the component names and values on my board so it's the same size? I tried a group select with the Info tool, but that didn't work. Only one item was changed.
On 05/05/2014 01:36 AM, Lorenz wrote:
Chuck Huber wrote:
Thus, after you have all your text selected into a group, you can add
change ratio 14 (C>0 0);
the 'C' modifier is not needed for group actions on the command line.
While a right click (or 'ctrl right click' if
Option.ToggleCtrlForGroupSelectionAndContextMenu is set to 1)
performed with the mouse would open a context menu, this makes no
sense when performing a simulated right click from the command line.
I tried it with setting the option to 1 and 0. You're right - the 'C'
is not required in either case.
I guess I've always used it only because that's what was required with
the mouse.
So this means that all right clicks from the command line operate on the
group regardless of the presence or absence of the 'C', and regardless
of the setting of Option.ToggleCtrlForGroupSelectionAndContextMenu in
~/.eaglerc.
This is good to know.
Thanks,
- Chuck