EAGLE User Support (English) Sega Genesis controller button contact in eagle?
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 580 views
  • Users 0 members are here
Related

Sega Genesis controller button contact in eagle?

Former Member
Former Member over 11 years ago

I need to make a Sega Genesis controller button contact in eagle. This looks like a circle with a hole on one side and a smaller circle in the center. These are the two contacts, so when the button is pressed pin1 in connected to pin 2. I see through-hole and SMD pads in the library tool, but not sure how to draw these odd shapes to make a custom pad. Any ideas?

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 3/05/2014 8:50 a.m., David Frost wrote:

    I need to make a Sega Genesis controller button contact in eagle. This

    looks like a circle with a hole on one side and a smaller circle in the

    center. These are the two contacts, so when the button is pressed pin1

    in connected to pin 2. I see through-hole and SMD pads in the library

    tool, but not sure how to draw these odd shapes to make a custom pad.

    Any ideas?

     

     

    First read HELP> PAD> Arbitrary Pad Shapes

    Those are the rules for creating an Arbitrary Pad Shape.

     

    Also, you will likely need to pick up the skills to form arcs using the

    WIRE command and the CTL key. Read HELP > WIRE > Drawing Arcs.

     

    Polygons can be time consuming so you have to be smart in the way you work.

     

    You could do it along these lines. Paste into the library editor  the

    lines in Upper case that follow so you can see the process.

     

    Open your library and start a new package

    Lay down some guides

    GRID MM; SET WIRE_BEND 2; CHANGE LAYER 51; WIRE 0 (0 10)(0 -10); WIRE 0

    (-10 0)(10 0);

    Lay down a guide for the outer annulus

    CIRCLE 2 (0 0)(4 0);

    Build a stick polygon roughly. We'll make the polygon wire

    8mil(0.2032mm) wide

    CHANGE WIDTH 0.2032mm;

    CHANGE LAYER 1;

    POLYGON 0.2032 (-5 .5)(-3 .5)(0 3)(3 0)(0 -3)(-3 -.5)(-5 0)(0 -5)(5 0)(0

    5)(-5 .5);

    Now use the 'Info' tool and change the 'Curve' of the long sides of the

    polygon to match the guiding circle. The outer sides will need to be

    made 90 and the inner sides -90 to get the curves bending the correct way.

    Next make the grid finest so we can match the rough polygon to the circle

    GRID FINEST;

    Now, at the orthogonal positions move the polygon to match the circle.

    Pay some attention to getting the join on the left looking good but

    there is a goal of not having the points overlap more than 49% or the

    wire width as the polygon wont like that. At the finest resolution there

    is a low change of this happening.

    Now you need to place a SMD within the polygon for a track on the board

    to connect to.

    SMD 1 1 (-4 0);

     

    You need to keep the solder mask off the contact so add a circle on that

    layer.

    CHANGE LAYER 29; CIRCLE 0 (0 0) (0 5.1);

    Look at the 'Information' of the SMD and un-check 'Thermals', 'Cream',

    and 'Stop'.

     

    The center contact can be done with a single SMD with 100% rounding or a

    polygon surrounding a smaller SMD. I'll leave that to you.

     

    HTH

    Warren