Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Multi-part component simulation with LTSpice
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 1944 views
  • Users 0 members are here
  • ltspice
  • eagle
  • multi-part
Related

Multi-part component simulation with LTSpice

Former Member
Former Member over 11 years ago

Hi,

 

I would like to simulate my circuit containing multiple opamps (AD8656) residing in one common package. I have created the library in Eagle for the component containing both parts (2 symbols, 1 package).

I was able to export the corresponding LTspice library, but only the first opamp simulation works. The spice model contains the subcircuit for one opamp only.

Eagle exported the two parts into separate LTSpice libraries AD8656G$1.asy and AD8656G$2.asy.

If I look into the second library file (AD8656G$2.asy), The part has no V+ and V- pins assigned, therefore it does not work.

 

How can I create and export a multi-part component to work with LTSpice?

 

Thanks,

  • Sign in to reply
  • Cancel
  • Richard_H
    0 Richard_H over 11 years ago

    What is the difference between the two opamps?

    Do you see the power pins in the EAGLE schematic or are these hidden pins? Maybe that's the problem and you have to INVOKE the power gates into EAGLE schematic?....

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Richard_H

    The two opamps are exactly the same. The power pins are only on the first part in the eagle schematic. I have tried to draw also power pins on the second opamp in the Eagle library editor, but these pins would be connected on the same power pads of the common package. Eagle does not allow this, since these package pads are already connected to the power pins from the first opamp (there would be more pins on the two opamps, than pads on the package).

    What am I doing wrong?

     

    Best regards,

    Zoltan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 11 years ago in reply to Former Member

    Hi,

     

    please use the INVOKE command in EAGLE and click onto the opamp with the missing pwr pins. Select the gate from the list and place it and connect the pins. Now it should work.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Richard_H

    Hi Richard,

     

    thanks for the answer, but that does not help. First of all, I have no separete power gate in my component lib. If I would create one, it will be even worse, because Eagle would export it as a separate LTSpice component (.asy).

    Please find my files attached.

    adtest.lbr - the Eagle library containing the opamps (ADTEST).

    ADTESTG$1.asy, ADTESTG$2.asy - the two LTSpice components generated by Eagle. If you compare the two files, you will see, that the G$2 does not have any connection the V+ and V-.

    adtest2.asc - the LTSpice test schematic exported from Eagle. The output signal on both opamps should be the same, but it is not, because the second opamp has no power.

     

    Could you please have a look at it?

     

    Thanks,

    Zoltan

    Attachments:
    adtest.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 11 years ago in reply to Former Member

    Hi Zoltan,

     

    the problem seems to be that LT Spice can't handle compnents that consist of more than one gate. So your opamp has to have both gates in one common symbol. If you 'ld change the library definition in EGALE it should work with LT Spice.


    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Richard_H

    Hi Richard,

     

    I can change the library to contain only one gate, but then I also have to change the spice model description, to contain something like a "double opamp". I am not a spice expert, so could you please help with this change? Is it possible at all to have two opamps in one spice subcircuit?

     

    Best regards,

    Zoltan