EAGLE User Support (English) Increase space between polygon and traces in v6.5
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 399 views
  • Users 0 members are here
  • polygon
Related

Increase space between polygon and traces in v6.5

Former Member
Former Member over 11 years ago

Greetings,

 

I'd like to keep a solid polygon further from my ckt board traces because I'm having to use two layers (per side) of overhead view-graph sheeting printed on by a laser printer. (one layer is a bit thin). Although the little HP1102 printer is really excellent, the printouts have some, almost random minor stretching, requiring very careful registration of "drillaid" holes. It's possible for parallel traces to become a couple of mils misaligned, so that the polygon ULP fills in a long sliver of wedge which can lead to inadequate/clearance etch.

 

I've tried all the permutations of toolbar spacing/line thickness/ etc, with all polygons showing the same tight spacing next to the traces, and I can't seem to get v6.5 to actually drop the orphan bits of polygon.

 

Can any set me straight as what I'm doing wrong?

 

Thanks in advance,

 

Frank Brasington

Satellite Beach, Florida

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    Am 18.05.2014 22:00, schrieb Frank Brasingron:

    Greetings,

     

    I'd like to keep a solid polygon further from my ckt board traces

    because I'm having to use two layers (per side) of overhead view-graph

    sheeting printed on by a laser printer. (one layer is a bit thin).

    Although the little HP1102 printer is really excellent, the printouts

    have some, almost random minor stretching, requiring very careful

    registration of "drillaid" holes. It's possible for parallel traces to

    become a couple of mils misaligned, so that the polygon ULP fills in a

    long sliver of wedge which can lead to inadequate/clearance etch.

     

    I've tried all the permutations of toolbar spacing/line thickness/ etc,

    with all polygons showing the same tight spacing next to the traces, and

    I can't seem to get v6.5 to actually drop the orphan bits of polygon.

     

    Can any set me straight as what I'm doing wrong?

     

    Thanks in advance,

     

    Frank Brasington

    Satellite Beach, Florida

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/113117

     

     

    change isolate.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    Am 18.05.2014 22:00, schrieb Frank Brasingron:

    Greetings,

     

    I'd like to keep a solid polygon further from my ckt board traces

    because I'm having to use two layers (per side) of overhead view-graph

    sheeting printed on by a laser printer. (one layer is a bit thin).

    Although the little HP1102 printer is really excellent, the printouts

    have some, almost random minor stretching, requiring very careful

    registration of "drillaid" holes. It's possible for parallel traces to

    become a couple of mils misaligned, so that the polygon ULP fills in a

    long sliver of wedge which can lead to inadequate/clearance etch.

     

    I've tried all the permutations of toolbar spacing/line thickness/ etc,

    with all polygons showing the same tight spacing next to the traces, and

    I can't seem to get v6.5 to actually drop the orphan bits of polygon.

     

    Can any set me straight as what I'm doing wrong?

     

    Thanks in advance,

     

    Frank Brasington

    Satellite Beach, Florida

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/113117

     

     

    change isolate.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag