EAGLE User Support (English) Kelvin connection or different ground connection
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
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 181 subscribers
  • Views 1885 views
  • Users 0 members are here
Related

Kelvin connection or different ground connection

kikoun
kikoun over 11 years ago

Hello,

 

I have a suggestion that could help us when we route kelvin connections or when we have to connect 2 separates ground planes in only one point ("star" connection). For example when we had to connect two ground GND-logic and GND_ANALOG  in one point only under the ADC....

For this kind of situation, even if all connexions must be connected together, some of them play different roles and could have different parameters (minimum width for kelvin connection).

 

Today I only found 2 ways for doing this:

1) On a schematic side,  I use one single net (same name). With this approach, on the board side, Eagle consider that all must be electrically connected. That is gread for DRC, but I have to manually check that the separation is correctly done, and some time I must add cutoff polygon (specially for GND planes). I also have no possibility to define different min width (same net = same class), ....

 

2) Or I use 2 different nets, and a "kelvin connection part"  that I have build in my library. Finally Eagle consider the 2 sides of this component as 2 different nets. Great, BUT, DRC is not really happy when I connect, the 2 nets with a manually added copper polygon or wire.

 

That I'm suggesting is:

I think that the best approach is to consider that we used different nets (different names) that we connect together with one special component. In schematic, these nets are totally independent (as in my solution 2). In broad, the package associated to this component would be a special package, that we can placed and locked like the other packages. But this package will take the form of a polygon (or at least a rectangle), We simply place this polygon (or rectangle) exactly where we want the connection of these 2 nets. This special polygon, will simple indicate to EAGLE (DRC and auto-router) that in this area and in this area only, these 2 nets must be proceed as only one net. The polygon let us decide the form of the connection.

 

In this way, it's easy to separate the 2 signals in schematic and in board. In the board we can decide where and how the connection is made. The DRC don't report any stupids error. And the DRC check the separation (isolate, with,...) of the to net, except under our special component.

 

Guillaume Barrey

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 11 years ago

    On 05/19/2014 07:40 AM, Guillaume barrey wrote:

    Hello,

     

    I have a suggestion that could help us when we route kelvin connections

    or when we have to connect 2 separates ground planes in only one point

    ("star" connection). For example when we had to connect two ground

    GND-logic and GND_ANALOG  in one point only under the ADC....

    For this kind of situation, even if all connexions must be connected

    together, some of them play different roles and could have different

    parameters (minimum width for kelvin connection).

     

    Today I only found 2 ways for doing this:

    1) On a schematic side,  I use one single net (same name). With this

    approach, on the board side, Eagle consider that all must be

    electrically connected. That is gread for DRC, but I have to manually

    check that the separation is correctly done, and some time I must add

    cutoff polygon (specially for GND planes). I also have no possibility to

    define different min width (same net = same class), ....

     

    2) Or I use 2 different nets, and a "kelvin connection part"  that I

    have build in my library. Finally Eagle consider the 2 sides of this

    component as 2 different nets. Great, BUT, DRC is not really happy when

    I connect, the 2 nets with a manually added copper polygon or wire.

     

    Have you looked at shorts.lbr in the download section?

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kikoun
    0 kikoun over 11 years ago in reply to dukepro

    Hi Chuck,

    Thank you for your answer.

    Chuck Huber a écrit:

     

    Have you looked at shorts.lbr in the download section?

     

    HTH,

        - Chuck

     

     

    I didn't know this lbr exist, but it's only an example of my solution #2. And it doesn't solve the all the problems:

     

    First problem and major one, DRC will report overlaps and clearance errors. In the case of the SHORT_ALL-50 Pachage (from SHORT.lbr) it's 4 overlaps errors per outer layers and 1 clearance error per inner layer) so 14 errors for a 6 layers. I'm designing a 6 layer board with 12 kelvin connections + one link between 2 GND... I let you do the math... 

    Ok it's possible to approve errors... But, each time you move one of these the package, the errors will appear again. So you approve again, again..... If you approve too many errors, one day you approve the wrong one without notice... and Ouch ! it can be very expansive when you work on a 6 layer prototype !

    According to me, the point of running DRC is not missing any potential problem, so DRC should report as errors only real errors.

    If we had the ability to disable some checking when we create a package (or at least ask to transform errors in to warning), we could found a way to solve this problem. Or maybe, an other elegant way could be to use "@" to name the pin. For example, If in the lbr we name the pins P@1 and P@2, Eagle would consider that these pins are electrically connected, so the DRU will skip clearance check. I already tried... But no...


    Second problem, like symbol in a schematic, I don't want to have all these kinds of component in the BOM. But this could be solve by adding an option "include/don't include in bom" for each component we create in library. This could be a great idea and very useful for other kind of components (card-edge connectors, etc... but it's an other subject.).

     

    Last problem, is that we had to build a package for each situation (depending on the wires width, or if the overlap is between 2 wires, 1 wire and a polygon, etc...)

    That why I suggest a polygon that we could draw. But this limitation is not really a big issue (for me).

     

    I think, that we already have in Eagle almost all we need to solve the 2 first problems. Just a couple of little things missing.

     

    Guillaume Barrey

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kikoun
    0 kikoun over 11 years ago in reply to dukepro

    Hi Chuck,

    Thank you for your answer.

    Chuck Huber a écrit:

     

    Have you looked at shorts.lbr in the download section?

     

    HTH,

        - Chuck

     

     

    I didn't know this lbr exist, but it's only an example of my solution #2. And it doesn't solve the all the problems:

     

    First problem and major one, DRC will report overlaps and clearance errors. In the case of the SHORT_ALL-50 Pachage (from SHORT.lbr) it's 4 overlaps errors per outer layers and 1 clearance error per inner layer) so 14 errors for a 6 layers. I'm designing a 6 layer board with 12 kelvin connections + one link between 2 GND... I let you do the math... 

    Ok it's possible to approve errors... But, each time you move one of these the package, the errors will appear again. So you approve again, again..... If you approve too many errors, one day you approve the wrong one without notice... and Ouch ! it can be very expansive when you work on a 6 layer prototype !

    According to me, the point of running DRC is not missing any potential problem, so DRC should report as errors only real errors.

    If we had the ability to disable some checking when we create a package (or at least ask to transform errors in to warning), we could found a way to solve this problem. Or maybe, an other elegant way could be to use "@" to name the pin. For example, If in the lbr we name the pins P@1 and P@2, Eagle would consider that these pins are electrically connected, so the DRU will skip clearance check. I already tried... But no...


    Second problem, like symbol in a schematic, I don't want to have all these kinds of component in the BOM. But this could be solve by adding an option "include/don't include in bom" for each component we create in library. This could be a great idea and very useful for other kind of components (card-edge connectors, etc... but it's an other subject.).

     

    Last problem, is that we had to build a package for each situation (depending on the wires width, or if the overlap is between 2 wires, 1 wire and a polygon, etc...)

    That why I suggest a polygon that we could draw. But this limitation is not really a big issue (for me).

     

    I think, that we already have in Eagle almost all we need to solve the 2 first problems. Just a couple of little things missing.

     

    Guillaume Barrey

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to kikoun

    Guillaume barrey wrote on Mon, 19 May 2014 12:56

    First problem and major one, DRC will report overlaps and clearance

    errors. In the case of the SHORT_ALL-50 Pachage (from SHORT.lbr) it's

    4

    overlaps errors per outer layers and 1 clearance error per inner

    layer)

    so 14 errors for a 6 layers. I'm designing a 6 layer board with 12

    kelvin connections + one link between 2 GND... I let you do the math...

     

    Yup, that's a pain.  There is a long standing request to be able to define

    in the package whether the DRC should flag overlap and clearance errors

    within a package.

     

    Quote:

    Ok it's possible to approve errors... But, each time you move one of

    these the package, the errors will appear again.

     

    Right, so don't do that.  Generally the workflow is to do all placement,

    then routing.  Occassionaly you do want to move something around as you see

    issues in placement, but that should be limited.  If you find yourself

    moving things a lot, then you should start by doing a better job of

    placement next time.

     

    Quote:

    like symbol in a schematic, I don't want to have all

    these kinds of component in the BOM.

     

    From the SHORT_ALL-50 name of one of the shorts, this seems to be my shorts

    library that someone uploaded to the CadSoft web site.  If so, these

    devices will already have a BOM attribute with value "no".  Take a look.

    That's how my automatic BOM generation system knows to not include these

    shorts in the BOM.  If this attribute isn't set, then either it's someone

    else's library or a very old version of mine.  You can get my latest

    version at http://www.embedinc.com/pic/dload.htm.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kikoun
    0 kikoun over 11 years ago in reply to autodeskguest

    Hi,

    thank you for your answers

    CadSoft Guest a écrit:

     

    Yup, that's a pain.  There is a long standing request to be able to define

    in the package whether the DRC should flag overlap and clearance errors

    within a package.

     

    That would be a great evolution. image

    Quote:

    Ok it's possible to approve errors... But, each time you move one of

    these the package, the errors will appear again.

     

    Right, so don't do that.  Generally the work-flow is to do all placement,

    then routing.  Occasionally you do want to move something around as you see

    issues in placement, but that should be limited.  If you find yourself

    moving things a lot, then you should start by doing a better job of

    placement next time.

    You right, the work-flow is to do a good placement first. And if I start some routing before a complete placing, it's only a quick crappy routing image, just for checking if there is enough room for routing. And I un-route it... image

    And the DRC comes later in the work-flow. So for me the "move around" it's not really an issue. It's just that if it's append, you have to approve errors again and be very carrefull when you re-approve errors. And in that case you have 12 errors for one little kelvin connections.

     

    I also always  re-check the my 'approved errors' at the end of the job, but like I says they are too numerous ! (precisely on my current board with 12 Kelvin connections). So Please Mr Cadsoft, We Beg you for this ability to flag errors in lbr packages !!!!

     

    From the SHORT_ALL-50 name of one of the shorts, this seems to be my shorts

    library that someone uploaded to the CadSoft web site.  If so, these

    devices will already have a BOM attribute with value "no".  Take a look.

    That's how my automatic BOM generation system knows to not include these

    shorts in the BOM.  If this attribute isn't set, then either it's someone

    else's library or a very old version of mine.  You can get my latest

    version at http://www.embedinc.com/pic/dload.htm.

     

    I download the library on the CadSoft web site, and the BOM attribute is already set to "no". But the BOM.ulp (eagle-6.5.0) or bom_w_attr_v2.ulp from cadsoft generate a bom with the "SHORT" device. Witch ulp you use ?

     

    Guillaume Barrey

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to kikoun

    Guillaume barrey wrote on Mon, 19 May 2014 14:47

    I download the library on the CadSoft web site, and the BOM attribute

    is

    already set to "no".

     

     

    That definitely sounds like my library.  I hope whoever uploaded it to the

    CadSoft web site gave me proper attribution.  I distrubute lots of my stuff

    for free, so I don't mind there being copies out there, but I do want

    people to know where they came from.  If this hasn't been done, CadSoft is

    violating my copyright.

     

    Quote:

    But the BOM.ulp (eagle-6.5.0) or *bom_w_attr_v2.ulp

    (http://www.cadsoftusa.com/downloads/file/bom_w_attr_v2.ulp)* from

    cadsoft generate a bom with the "SHORT" device. Witch ulp you use ?

     

     

    My own, of course, which is also included in my Eagle Tools Release along

    with the shorts library and all the other stuff.  I have had a BOM

    generation system using the user-definable attributes that were first

    available in version 5.  Unfortunately when CadSoft created their own, they

    used different conventions.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kikoun
    0 kikoun over 11 years ago in reply to autodeskguest

    I never take time to learn ulp language.... I think it's time for me to look at it.

    I will try to adapt the BOM.ulp (eagle-6.5.0) or bom_w_attr_v2.ulp to my need. That will be a good first project to learn ulp !

     

    I hope one day we could have the ability to flag DRC errors for library package...

     

    Thank you again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 11 years ago in reply to autodeskguest

    On 05/19/2014 03:24 PM, Olin Lathrop wrote:

    Guillaume barrey wrote on Mon, 19 May 2014 14:47

    I download the library on the CadSoft web site, and the BOM attribute

    is

    already set to "no".

     

    That definitely sounds like my library.  I hope whoever uploaded it to the

    CadSoft web site gave me proper attribution.

     

    I uploaded it with several additional packages.  And you're right, I

    should have mentioned its origination.

     

    Let it hereby be publicly known that Olin Lathrop is a contributor to

    the shorts.lbr library as posted on the Cadsoft web site.

     

    I wonder if Jorge can update the description of the download.

     

    Best regards,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to dukepro

     

     

    I uploaded it with several additional packages.  And you're right, I

    should have mentioned its origination.

     

    Let it hereby be publicly known that Olin Lathrop is a contributor to

    the shorts.lbr library as posted on the Cadsoft web site.

     

    I wonder if Jorge can update the description of the download.

     

    Best regards,

         - Chuck

     

    Hi Chuck,

     

    I don't have rights to alter anything on the site. I believe under you

    profile under Cadsoftusa.com you may be able to edit it. If not contact

    ric@cadsoft.de and he'll correct it for you.

     

    hth,

    Jorge Garcia