EAGLE User Support (English) Kelvin connection or different ground connection
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
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 181 subscribers
  • Views 1886 views
  • Users 0 members are here
Related

Kelvin connection or different ground connection

kikoun
kikoun over 11 years ago

Hello,

 

I have a suggestion that could help us when we route kelvin connections or when we have to connect 2 separates ground planes in only one point ("star" connection). For example when we had to connect two ground GND-logic and GND_ANALOG  in one point only under the ADC....

For this kind of situation, even if all connexions must be connected together, some of them play different roles and could have different parameters (minimum width for kelvin connection).

 

Today I only found 2 ways for doing this:

1) On a schematic side,  I use one single net (same name). With this approach, on the board side, Eagle consider that all must be electrically connected. That is gread for DRC, but I have to manually check that the separation is correctly done, and some time I must add cutoff polygon (specially for GND planes). I also have no possibility to define different min width (same net = same class), ....

 

2) Or I use 2 different nets, and a "kelvin connection part"  that I have build in my library. Finally Eagle consider the 2 sides of this component as 2 different nets. Great, BUT, DRC is not really happy when I connect, the 2 nets with a manually added copper polygon or wire.

 

That I'm suggesting is:

I think that the best approach is to consider that we used different nets (different names) that we connect together with one special component. In schematic, these nets are totally independent (as in my solution 2). In broad, the package associated to this component would be a special package, that we can placed and locked like the other packages. But this package will take the form of a polygon (or at least a rectangle), We simply place this polygon (or rectangle) exactly where we want the connection of these 2 nets. This special polygon, will simple indicate to EAGLE (DRC and auto-router) that in this area and in this area only, these 2 nets must be proceed as only one net. The polygon let us decide the form of the connection.

 

In this way, it's easy to separate the 2 signals in schematic and in board. In the board we can decide where and how the connection is made. The DRC don't report any stupids error. And the DRC check the separation (isolate, with,...) of the to net, except under our special component.

 

Guillaume Barrey

  • Sign in to reply
  • Cancel
Parents
  • kikoun
    0 kikoun over 11 years ago

    Hi,

    I'm working on new board with  a lot of Kelvin connection, and half of them are connected to GND (measuring current, in low side resistor) If I use separate names I will have a large amount of 'fake error'.If I use the same name, I will have to add a lot of restrict and cutout polygon to avoid mixup....

    Whatever I choose I'm screwed with a 'workaround' solution.

    It's a really pain image!!!

    It's seems that I'm not the only one to complain about it.

     

    Is someone know if a feature to solve that problem of start connection/kelvin connection is planed ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kikoun
    0 kikoun over 11 years ago

    Hi,

    I'm working on new board with  a lot of Kelvin connection, and half of them are connected to GND (measuring current, in low side resistor) If I use separate names I will have a large amount of 'fake error'.If I use the same name, I will have to add a lot of restrict and cutout polygon to avoid mixup....

    Whatever I choose I'm screwed with a 'workaround' solution.

    It's a really pain image!!!

    It's seems that I'm not the only one to complain about it.

     

    Is someone know if a feature to solve that problem of start connection/kelvin connection is planed ?