EAGLE User Support (English) EAGLE update26.exe help
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 535 views
  • Users 0 members are here
  • eagle
  • update26
Related

EAGLE update26.exe help

Former Member
Former Member over 11 years ago

Hello,

As a new EAGLE user, I need to view some schematics (.sch) in order to build an electroencephalograph. The problem is that they are old, from around 2003.  I have the light edition of EAGLE 6.6.0 for OS X. In order to view the old files, the manual says I must run the program "update26.exe," which can be found in the "bin" folder of my EAGLE download. However, the program is not there, nor is it anywhere else in the download. Could it possibly be called something else, do I need to have the full version, or am I just being stupid?

Thank you.

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    You may have a bad download of Eagle. The file is still there where it

    is said to be. Once you get it have a read of the following so you use

    update26.exe correctly.

     

    http://ftp.cadsoft.de/faq.htm.en

     

    9. Converting Older Files From EAGLE Versions Prior 2.6 to 3.xx/4.xx/5.xx:

     

     

    All the best

    Warren

     

     

    On 10/06/2014 7:19 a.m., Christopher Dowd wrote:

    Hello,

    As a new EAGLE user, I need to view some schematics (.sch) in order to

    build an electroencephalograph. The problem is that they are old, from

    around 2003.  I have the light edition of EAGLE 6.6.0. In order to view

    the old files, the manual says I must run the program "update26.exe,"

    which can be found in the "bin" folder of my EAGLE download. However,

    the program is not there, nor is it anywhere else in the download. Could

    it possibly be called something else, do I need to have the full

    version, or am I just being stupid?

    Thank you.