Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How to I prevent thermal connections on 0402 packages (to, in turn, mitigate tombstoning)?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 594 views
  • Users 0 members are here
  • thermals
  • tombstone
  • 0402
Related

How to I prevent thermal connections on 0402 packages (to, in turn, mitigate tombstoning)?

icefield
icefield over 12 years ago

For routing to 0402 parts, it is important to keep the traces balanced in terms of orientation and copper load so that both sides of the 0402 melt and solidify at the same time. Otherwise tombstoning becomes an issue. If one end of an 0402 part is connected to a polygon fill signal (e.g. ground), how do I prevent any connections from occurring? The default is 3 connections to the ground plane, but (for this package only) I want NO connections. I want to route these parts manually.

 

Covering the pad with a tRestrict rectangle seems to do the trick, but this results in Restrict errors under DRC when you connect traces to the pad, so it's not ideal. Are there any other solutions?

 

This same issue would also apply to smaller parts (e.g. 0201, 01005)

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 06/20/2014 05:33 PM, Erik Blake wrote:

    Covering the pad with a tRestrict rectangle seems to do the trick, but

    this results in Restrict errors under DRC when you connect traces to the

    pad, so it's not ideal. Are there any other solutions?

    Use a thin tRestrict wire just outside the pad on three sides on as needed.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • ootbrobo
    0 ootbrobo over 12 years ago in reply to autodeskguest

    1) You can approve that particular error the DRC throws, since you know it is not a problem.  This approval will remain until you move the part or trace (I believe).

     

    2) Use restrict lines around the connection you would like to make at the board level.  You just have to leave a gap for the trace/thermal, so that the DRC will not throw an error.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • icefield
    0 icefield over 12 years ago in reply to ootbrobo

    Thanks Tim & guest.

     

    I will use the tRestrict line around the pads. Tim's option 1 is what I'm dealing with now, but there are hundreds of those tRestrict errors and there is no easy way to approve a subset of tRestrict errors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • icefield
    0 icefield over 12 years ago in reply to ootbrobo

    Thanks Tim & guest.

     

    I will use the tRestrict line around the pads. Tim's option 1 is what I'm dealing with now, but there are hundreds of those tRestrict errors and there is no easy way to approve a subset of tRestrict errors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • icefield
    0 icefield over 12 years ago in reply to ootbrobo

    Yes, I know about double-clicking. But doing this for hundreds of errors, and all the associated mouse movements to click on "approve" and then back to the list quickly gets tiresome. Older versions of Eagle (I'm using 5.11) used to approve DRC errors with a middle-mouse click, but that no longer works - that was "super fast" because you did not have to move the mouse very much. And if you make an adjustment to the DRC rules, all the approvals get deleted and you have to start over. "Guest's" suggestion of a zero-width line around three sides of the pads in question worked wonderfully.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ootbrobo
    0 ootbrobo over 12 years ago in reply to icefield

    You are double clicking on the DRC errors right?  Eagle will bring the individual error center screen and highlight it.  You can go through and approve the errors super fast.