EAGLE User Support (English) Custom library connector, pins don't connect on board
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
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 736 views
  • Users 0 members are here
  • library
Related

Custom library connector, pins don't connect on board

ckambiselis
ckambiselis over 11 years ago

Hello,

 

I have bought some HDMI board connectors for a project and I have to build a library for it since I can't find an HDMI connector library.

 

I have created the library (device, package, symbol) and connected the package SMD pads with pin of the symbol, but when I wire the pins with a connector on the schematic, the wires don't appear on the board side. Am I missing something, this is my first custom library.

 

Thanks

Oscar

Attachments:
HDMI.zip
  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 22/06/14 12:23, Christos Oscar Kambiselis wrote:

     

    I have created the library (device, package, symbol) and connected the

    package SMD pads with pin of the symbol, but when I wire the pins with a

    connector on the schematic, the wires don't appear on the board side. Am

    I missing something, this is my first custom library.

     

    The usual reason for this is that you failed to put your symbol pins

    aligned on the 0.1" grid used in schematics. I've not got V6 installed

    here but looking at the XML you seem to have defined them on a 2.54 inch

    grid by mistake. Of course I could just be totally misreading the XML!

     

    Cheers,

    Rob

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    Your library is fine

     

    The problem is the nets do not attach to the pins on the other device.

    You likely connected the devices using the WIRE tool instead of the NET

    tool.

     

    You can verify the non connection by moving the part. The nets should stay

    attached  to the part you are moving.

     

    To fix, simply move the net end away and then back to the pin

     

    HTH

    Warren

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to autodeskguest

    I'm using a 0.1 inch grid, the 2.54 you see in the xml must be the mm

    value. But made me think and I checked with another connector and it

    works fine, seems that someone else didn't make a good job, well, thank

    anyway.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/117937

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ckambiselis
    0 ckambiselis over 11 years ago in reply to autodeskguest

    I'm using a 0.1 inch grid, the 2.54 you see in the xml must be the mm value. The nets where not visible on the board, but you first reply made me think and I checked with another connector and it works fine, seems that someone else didn't do a good job, well, thanks anyway.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to autodeskguest

    Warren Brayshaw wrote:

    Your library is fine

     

    The problem is the nets do not attach to the pins on the other device.

    You likely connected the devices using the WIRE tool instead of the NET

    tool.

     

    You can verify the non connection by moving the part. The nets should stay

    attached  to the part you are moving.

     

    To fix, simply move the net end away and then back to the pin

     

    not quite ...

     

    you need to pick up the part and drop it in place, to make the nets

    connect.

    --

     

    Lorenz