EAGLE User Support (English) Error Messages
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
  • State Not Answered
  • Replies 5 replies
  • Subscribers 179 subscribers
  • Views 504 views
  • Users 0 members are here
Related

Error Messages

Former Member
Former Member over 11 years ago

Attached are two screen shots of ERC error messages and the associated schematic section. These errors all result in no physical connection being made in the  board layout so I need to solve them and understand what's happening. The F1 Help apparently doesn't provide and answer to these specific messages.

 

"XXX overlaps pin". I have removed and remade this connection a half dozen times being careful to make sure the "wire" does not overlap the end of the "pin" but I keep getting them.

 

"Only INPUT pins on N$3". This is the input side of a 7805 VR being connected to the 5V output side of a barrel jack.

 

"Unconnected pin on U$1 NEG" but it certainly looks connected to me. I created the Library part and I have double checked that it has the Physical Pin "NEG" connected to the Logical Pin "POS".

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • AnalogNotes
    0 AnalogNotes over 11 years ago

    We're making a Costco trip in a few minutes here, but before I run out, I thought I'd at least ask if you've used the move tool and dragged your part around a bit.  I always do that to see if all of the connections are actually attached and move with the part.  Sometimes the net isn't actually connected and will just sit there when you move the part.  Hit the ESC key to abort the move, or you can just use UNDO after moving the part...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to AnalogNotes

    Thanks, that did help identify the situation. I still don't understand what causes it but I was able to get them connected.

     

    Leaves me basically with the problem of the pins on the power jack and the 7850 still not connecting. But I think worst comes to worst I can manually route them on the board layout

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • AnalogNotes
    0 AnalogNotes over 11 years ago in reply to Former Member

    One of the recurring issues I've seen is that the schematic editor needs everything on .1" grid.  If the schematic grid is changed to something else for any reason, you'll have problems with connections...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to AnalogNotes

    Interesting, I'll keep that in mind, I may have modified the grid, I don't recall.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to AnalogNotes

    Interesting, I'll keep that in mind, I may have modified the grid, I don't recall.