EAGLE User Support (English) Connecting two separate nets to one junction.
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
  • State Not Answered
  • Replies 5 replies
  • Subscribers 178 subscribers
  • Views 1344 views
  • Users 0 members are here
Related

Connecting two separate nets to one junction.

Former Member
Former Member over 11 years ago

I'm trying to connect two different nets to one junction.  Each nets carries separate trace sizing due to amp draws from components.  How can I connect the two nets to one junction with out combining the nets? I would like to keep the nets separate to minimize trace size on the final pcb.

Thanks

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Cant you create a net with different size traces?

     

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 01/07/14 17:02, Brian Wilkins wrote:

    I'm trying to connect two different nets to one junction.  Each nets

    carries separate trace sizing due to amp draws from components.  How can

    I connect the two nets to one junction with out combining the nets? I

    would like to keep the nets separate to minimize trace size on the final

    pcb.

     

    This is a VFAQ! (Is there an FAQ page for this newsgroup anywhere?)

     

    Basically, if two nets are connected then they're the same net. To keep

    them separate you need to connect them only through a component. But

    since Eagle knows nothing about what components actually do, it's quite

    happy to accept a device which just wires things together. The normal

    trick is to create a device whose symbol is two pins connected together

    and whose package is two (SMD) pads coincident. This will create DRC

    errors but you can accept them and they go away.

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    Brian Wilkins wrote on Tue, 01 July 2014 12:02

    I'm trying to connect two different nets to one junction.  Each nets

    carries separate trace sizing due to amp draws from components.  How

    can

    I connect the two nets to one junction with out combining the nets?

     

     

    You can't.  Everything in a net is connected, which is not connected to any

    other net.  Remember that what order a line on a schematic connects to

    different pins has nothing to do with what order the trace on the PCB will

    eventually connect the same pins.

     

    As Rob has already said, you create separate nets for the traces you want

    different classes for, then connect them with a component that is just

    copper on the PCB.  This is exactly what my "shorts" library is for.  It is

    included in my Eagle Tools release at

    http://www.embedinc.com/pic/dload.htm.  They look like slightly thickened

    short lines on the schematic.

     

    The downside of this method is that you'll get lots of annoying DRC errors

    due to the overlaps between the pads in the short packages.  Maybe some day

    Eagle will finally have the ability to be told to ignore DRC error wholly

    within specific packages pre-approved for that purpose.  For now you'll

    have to approve all the errors.  If you move one of these short packages

    around on the PCB, then you'll have to approve them all over again.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to autodeskguest

    Actually, the link above is http://www.embedinc.com/pic/dload.htm  As

    shown, it includes the "." as part of the link which breaks it ... ain't

    technology wonderful??

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Thank you for the help.  I was able to use a generic component between the net connections.