Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Create part with multiple ground signals
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 2099 views
  • Users 0 members are here
Related

Create part with multiple ground signals

scott216
scott216 over 11 years ago

I made a part in my part library.  It has several ground pins that are already connected together within the part itself.  I named them GND@1, GND@2 and GND@3.  I also defined them all as swap level 1.  In my schematic and board, I am only using one of the 3 ground pins.  But in the board file, there are unrouted airwires between all 3 pins.  I don't need traces between them because they are already connected internally. Should I have created my part differently?  What's the best way to do something like this?  I'm using Eagle 6.5.0 on a Mac.

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Am 15.07.2014 01:23, schrieb scott216:

    I made a part in my part library.  It has several ground pins that are

    already connected together within the part itself.  I named them GND@1,

    GND@2 and GND@3.  I also defined them all as swap level 1.  In my

    schematic and board, I am only using one of the 3 ground pins.  But in

    the board file, there are unrouted airwires between all 3 pins.  I don't

    need traces between them because they are already connected internally.

    Should I have created my part differently?  What's the best way to do

    something like this?  I'm using Eagle 6.5.0 on a Mac.

     

    You can use one PIN named GND at the symbol, and on the CONNECT you can

    connect all 3 PADs on this GND pin by and switch the

    connection to ANY or ALL.

     

    Please read also

    HELP PIN

    HELP CONNECT

     

     

    ***

    Um das Original zu lesen, und auch zuverlässig angehängte Dateien

    bereitstellen zu können, benutzen Sie news.cadsoft.de und einen

    funktionierenden News-Reader wie Thunderbird!

    ***

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

     

    • The new EAGLE V7 has landed *

    ______________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschaeftsfuehrer: Thomas Liratsch, Mark Whiteling

    ______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • scott216
    0 scott216 over 11 years ago in reply to Former Member

    That worked great, thanks!