EAGLE User Support (English) Use a symbol without footprint in the schematic editor
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
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 2035 views
  • Users 0 members are here
Related

Use a symbol without footprint in the schematic editor

Former Member
Former Member over 11 years ago

Dear all,

 

I'm trying to create a schematic using several components with symbol only because I don't need the footprint for now. How can I use the component without the footprint in my schematic? When I try to add them, I got error.

Best,

Cortex

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member +1 suggested
    Hello Mario, The easiest thing to do is to draw a symbol without pins on it. This will avoid defining actual electrical connections and allow you to put it into a schematic without issue. Additionally…
  • autodeskguest
    0 autodeskguest over 11 years ago

    Mario Cortese wrote:

    I'm trying to create a schematic using several components with symbol

    only because I don't need the footprint for now. How can I use the

    component without the footprint in my schematic? When I try to add them,

    I got error.

     

    you have read the online help about the package command?

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    I'm a newbie of Eagle. Can you specify more clearly what do I have to do?

    M

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Does someone have any ideas?

    Please,

    best

    M

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    Hello Mario,

     

    The easiest thing to do is to draw a symbol without pins on it. This

    will avoid defining actual electrical connections and allow you to put

    it into a schematic without issue.

     

    Additionally, you could draw a normal symbol and in the device editor

    create an attribute called EXTERNAL, this tells EAGLE the component is

    off the board and therefore doesn't need a package.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer