EAGLE User Support (English) Beaglebone shield outline
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
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 178 subscribers
  • Views 831 views
  • Users 0 members are here
  • cape
  • Black
  • outline
  • BeagleBone
  • ground
  • shield
Related

Beaglebone shield outline

dcdc
dcdc over 11 years ago

Hi all

 

I'm a newbie to this stuff, but have been watching lots of videos and blogs etc. I'm trying to design a cape for the beaglebone black, using the "beaglebone_shield" from the adafruit library. What I wasn't expecting is for the shield's outline to be cut out of the ground plane. Is that right or am I doing something wrong?

image

 

thanks,

Danny

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 11 years ago

    Hi Danny,

    I have created a BBB cape template schematic and board layout that I used to create a cape.

    The cape fits properly and works well. The holes actually line up properly despite how they look in the picture below. The template includes the standard cape EEPROM. I made the connector pads a bit smaller than some other templates so heavier traces could be routed between pads.

    The template is the same size as the BBB - not shortened to provide better access to buttons.

    If someone wants to explain the best way to publish this template project, I would consider making it available.

    The whole project will likely end up being published at some point.

    The project blog is here:

    Vehicle Simulator - VTR / RTR

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago

    Hi Danny,

    I have created a BBB cape template schematic and board layout that I used to create a cape.

    The cape fits properly and works well. The holes actually line up properly despite how they look in the picture below. The template includes the standard cape EEPROM. I made the connector pads a bit smaller than some other templates so heavier traces could be routed between pads.

    The template is the same size as the BBB - not shortened to provide better access to buttons.

    If someone wants to explain the best way to publish this template project, I would consider making it available.

    The whole project will likely end up being published at some point.

    The project blog is here:

    Vehicle Simulator - VTR / RTR