EAGLE User Support (English) Thermal Via's
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 180 subscribers
  • Views 268 views
  • Users 0 members are here
Related

Thermal Via's

GP100
GP100 over 11 years ago


Hi


We are using Eagle version 5,11 and are designing a small switcher PSU that utilises the Texas TPS54340 Device. Farnell part No 2255010.


I have downloaded the cad soft package for this device but have the following query.


In the data sheet it has a typical layout for the device. It shows thermal vias underneath the package through the central GND connection Pad. These are then connected to the GND plane on the lower side of the board to enhance the thermal properties of the device.


Is there any way of generating these thermal vias through the Gnd pad on the symbol? Each way that I seem to try these it clears the GND plane beneath or has an overlap error in the DRC.

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Am 01.08.2014 10:05, schrieb Gareth Pritchard:

     

    Hi

     

     

     

    We are using Eagle version 5,11 and are designing a small switcher PSU

    that utilises the Texas TPS54340 Device. Farnell part No 2255010.

     

     

    I have downloaded the cad soft package for this device but have the

    following query.

     

     

    In the data sheet it has a typical layout for the device. It shows

    thermal vias underneath the package through the central GND connection

    Pad. These are then connected to the GND plane on the lower side of the

    board to enhance the thermal properties of the device.

     

     

    Is there any way of generating these thermal vias through the Gnd pad on

    the symbol? Each way that I seem to try these it clears the GND plane

    beneath or has an overlap error in the DRC.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/122535

     

     

    Please send me the board and the library.

     

     

    ***

    Um das Original zu lesen, und auch zuverlässig angehängte Dateien

    bereitstellen zu können, benutzen Sie news.cadsoft.de und einen

    funktionierenden News-Reader wie Thunderbird!

    ***

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

     

    • The new EAGLE V7 has landed *

    ______________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschaeftsfuehrer: Thomas Liratsch, Mark Whiteling

    ______________________________________________________________