EAGLE User Support (English) Off-board connection of signals
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
  • State Not Answered
  • Replies 0 replies
  • Subscribers 178 subscribers
  • Views 199 views
  • Users 0 members are here
  • board
  • pcb_traces
Related

Off-board connection of signals

Former Member
Former Member over 11 years ago

Hi!

 

I am currently working on a shield for an Arduino Due board. The Due board has a couple pins which are connected to the 5V on the Arduino board. I wish to define these pins on my board as having the same net name and being connected externally (off-board). This way I could use the 5V from the closest source available. I have now realized this as adding an inner layer and connected the pins using this layer. This works for now but it may lead to confusion later.

I want to ask what is the best practice in this case?

Is there maybe a setting which I do not know about to define signals which are externally connected?

 

Thank you!