EAGLE User Support (English) How to add an existing schematic to a project
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
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 2678 views
  • Users 0 members are here
Related

How to add an existing schematic to a project

cosborne2000
cosborne2000 over 11 years ago

When starting a new project, how can I add an existing schematic into the project?

Another way of stating this-- if I have a schematic and board file, how can I add a project file to the directory so Eagle sees them as a project?

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 05/09/14 16:11, cosborne2000 wrote:

    When starting a new project, how can I add an existing schematic into

    the project?

     

    Open the project, then open the existing schematic. Then close the

    project (or close Eagle) and that schematic is now associated with the

    project. You may want to copy the .sch and .brd files into the project

    folder first.

     

    Another way of stating this-- if I have a schematic and board file, how

    can I add a project file to the directory so Eagle sees them as a

    project?

     

    Copy an eagle.epf file from another project into the same place as the

    schematic and board, and the folder becomes a project. You will have to

    open this project then open the correct schematic, to get round it being

    the wrong EPF. Unfortunately, while a completely empty epf file will

    make the folder look like a project, it won't be possible to open it.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    Hey, great - that was a question I have been meaning to ask for some time

    and was about to do so.  Glad to see others have the same questions I do

    !!

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.