Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) ring-shaped smd pad
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 190 subscribers
  • Views 2388 views
  • Users 0 members are here
  • pad
  • round
  • smd
  • circular
Related

ring-shaped smd pad

e14 Contributor
e14 Contributor over 12 years ago

I need to create 2 ring-shaped smd pads.

One with smaller diameter on bottom side and one with bigger diameter on top side.

Using a round polygon with inner cutout-polygon has no use. In lib or board the cutout-polygon is ignored.

 

As abstract:   how do you create a ring-shaped smd pad in the library?

 

Eagle 6.5.0

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    Oliver Schumann wrote on Tue, 09 September 2014 01:30

    I need to create 2 ring-shaped smd pads.

    One with smaller diameter on bottom side and one with bigger diameter

    on

    top side.

    Using a round polygon with inner cutout-polygon has no use. In lib or

    board the cutout-polygon is ignored.

     

    Eagle 6.5.0

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/125916

     

     

     

    Look in the HELP

    "Arbitrary Pad Shapes

    If the standard pad shapes are not sufficient for a particular package, you

    can create arbitrary pad shapes by drawing a polygon around a pad, or by

    drawing wires that have one end connected to the pad. "

     

    Depending on  the size the wire approach may be better than the polygon. In

    that case read about Wire in the help to make arcs.

     

    Let us know the sizes of your rings (diameter and width of the copper) and

    someone  will likely create examples for you to learn from

     

    HTH

    Warren

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    The polygon variant was not sufficient, because I need a hole in it.

    A circle didn't connect to the smd pad.

    But the wire made the job.

    Thanks for the hint.

     

    Oliver S. ISLE GmbH, Ilmenau.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kikoun
    0 kikoun over 12 years ago in reply to e14 Contributor

    Hi,

     

    You can do it with a polygon, but you have to start with an incomplete ring, because eagle will consider that you polygon command is ended to soon (look at the example...

    image

     

    Then you edit the polygon by moving the vertical line, in order to have the complete ring !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • yttrium
    0 yttrium over 9 years ago in reply to kikoun

    The complicated polygon here seems to be the best answer, though you can't let the two vertical top lines quite overlap or you will get an invalid polygon error.

    Using wires, circles, arcs, etc. overlapping a pad seems to be basically a hack and of limited use. The reason seems to be that only polygons can be part of a named net; the others can't.

    If you use polygons in your board they will not work right with a ring pad made of a wire. For example, I want my pad (connected to GND) to connect to my GND power plane. Nope, doesn't work. The power plane maintains a nice gap all around my ring and doesn't connect properly. With the polygon version it does, but it's much more annoying to draw than a circle.

     

    Can you EAGLE guys fix the cutout feature so it works for library parts? Thanks. (I'm still on version 7.1, so ignore if it has been fixed already.) Also, why can't wires and stuff be assigned to nets, like you can with vias and polygons?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • yttrium
    0 yttrium over 9 years ago in reply to kikoun

    The complicated polygon here seems to be the best answer, though you can't let the two vertical top lines quite overlap or you will get an invalid polygon error.

    Using wires, circles, arcs, etc. overlapping a pad seems to be basically a hack and of limited use. The reason seems to be that only polygons can be part of a named net; the others can't.

    If you use polygons in your board they will not work right with a ring pad made of a wire. For example, I want my pad (connected to GND) to connect to my GND power plane. Nope, doesn't work. The power plane maintains a nice gap all around my ring and doesn't connect properly. With the polygon version it does, but it's much more annoying to draw than a circle.

     

    Can you EAGLE guys fix the cutout feature so it works for library parts? Thanks. (I'm still on version 7.1, so ignore if it has been fixed already.) Also, why can't wires and stuff be assigned to nets, like you can with vias and polygons?