EAGLE User Support (English) Generating Gerber Files
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
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 482 views
  • Users 0 members are here
Related

Generating Gerber Files

Former Member
Former Member over 11 years ago

I've used Eagle v6 to create a small prototype 2-layer board and I'm having difficulties generating Gerber files.

After running the CAD Processor as a job (all layers selected) it only creates three very small files that don't have the extensions I expected. One file has no extension, the second is a .dri file and the third is .gpi. The only way I can generate the various files I think I need is to enter the respective file extension manually before running each section individually. When I run the CAM as a job, it appears to be overwriting or deleting the previous file in the Gerber_RS274X sequence. I installed Eagle 7 freeware edition and get the same issues. What am I doing wrong?

Thanks,

WaveGuide

  • Sign in to reply
  • Cancel
Parents
  • kikoun
    0 kikoun over 11 years ago

    Hi,

    In your job, you have to create a section for each file you want to create. for each section, you select the options and the layers corresponding to the gerber file you want to create, and define a destination file name using the place holder '%N ...

    You can have a look on the job examples installed with eagle.

    You must have a different name for each section. If you use the same name, each section will overwrite the previous gerber file !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kikoun

    Ah I see. The freeware version doesn't run the CAD in automatic mode. That explains my findings. Many thanks for clearing it up.

     

    WaveGuide

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to kikoun

    Ah I see. The freeware version doesn't run the CAD in automatic mode. That explains my findings. Many thanks for clearing it up.

     

    WaveGuide