Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) holes not in Excellon drill file
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 1178 views
  • Users 0 members are here
Related

holes not in Excellon drill file

e14 Contributor
e14 Contributor over 11 years ago

Hi all,

 

I attempted to send a manufacturer a drill file in Excellon format, but they informed me that several 0.6" holes I wanted drilled were not in the Excellon drill file.  I browsed through the file and it appears that they are not present.

 

I checked one of the holes and it is in the "holes" layer as a circle.  In one of the forums it is suggested that a circle in the holes layer is not correct.  http://www.element14.com/community/message/57758/l/conversion-to-excellon-problem#57758

 

Is there some magic to tell Eagle to place these holes in the Excellon drill file?

 

Thanks,

Jeremy

Attachments:
image
HeaterLEDBoard.drd.zip
  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to e14 Contributor

    On 25/09/14 23:24, Jeremy Dwyer wrote:

    Sounds good.  Out of curiosity, what if you want to do a custom cutout?

    Can this be done added in the drill file?  Sorry if this is a novice

    question.

     

    Custom shapes would not be in the drill file but rather in the milling

    layer. However, check with your board house because not all of them will

    handle milling on their low cost service. The point is that the holes

    layer, like the drill layer, defines things done with drills, which

    means only circular holes. Milling involves a different tool that has

    much better lateral stress handling and a completely different cutter.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to autodeskguest

    Quote:

    I checked one of the holes and it is in the "holes" layer as a circle.

     

    In one of the forums it is suggested that a circle in the holes layer

    is

    not correct.

     

     

    As rob said.

    Also, the holes layer does not display a circle but the symbol that relates

    to the diameter of the hole. Have a practice, display only the Hole layer

    and proceed to place holes of different diameters and see the symbol

    change.

     

    Next turn on the Dimension layer 20. and you will see the hole outline

    drawn. This depiction of the hole outline is used to keep other objects

    like polygon flood fills back from the hole as defined in the DRC

    settings.

     

    From the board you can go Options > Set... > Drill and manage the drill

    menu. Also there you can click on 'Set' to assign symbols to all the sizes

    used on your board.

     

     

    HTH

    Warren

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    Sounds good.  Out of curiosity, what if you want to do a custom cutout?  Can this be done added in the drill file?  Sorry if this is a novice question.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 25/09/14 19:02, Jeremy Dwyer wrote:

    I checked one of the holes and it is in the "holes" layer as a circle.

    In one of the forums it is suggested that a circle in the holes layer is

    not correct.

    http://www.element14.com/community/message/57758/l/conversion-to-excellon-problem#57758

    (/message/57758/l/conversion-to-excellon-problem#57758)

     

    Is there some magic to tell Eagle to place these holes in the Excellon

    drill file?

     

    The holes layer should not contain circles. It should contain holes.

    Only holes in the holes and drills layers will be included in the

    Excellon file. Note that pads and vias automatically create holes in the

    drills layer, whereas mounting holes for connectors are explicitly drawn

    as holes in the holes layer by the library package.

     

    If you have board mounting holes then you should draw them as a hole in

    the holes layer. It's common to also draw a circle in the dimension

    layer, and quite possibly a larger circle in the restrict and/or keepout

    layers. To this end it may be worth creating a mounting hole library

    part - or use one of the ones in the holes library.

     

    HTH

    Rob

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer