EAGLE User Support (English) I have stuck at the wire connections in the schematic, unable to join the connection between two pins of any component. Kindly help to resolve the problem. I am using Eagle 6.5
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 180 subscribers
  • Views 268 views
  • Users 0 members are here
Related

I have stuck at the wire connections in the schematic, unable to join the connection between two pins of any component. Kindly help to resolve the problem. I am using Eagle 6.5

harishzambani
harishzambani over 11 years ago

The wire connection in the schematic is not able to connect. but the same thing is getting done with the previous file.

 

Kindly suggest the solution. I am using Eagle 6.5

Attachments:
L298.sch.zip
  • Sign in to reply
  • Cancel
  • Richard_H
    0 Richard_H over 11 years ago

    Hi,

     

    you did not place the components in the 0.1 inch grid. All the symbols are defined in 0.1 inch grid and you should place them with this grid setting in the schematic.

     

    You could use snap-on-grid sch.ulp to correct this.

     

    Regards,

    Richard