EAGLE User Support (English) Repeatable Segfault when running Eagle CAM generation from command line
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
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 180 subscribers
  • Views 1178 views
  • Users 0 members are here
  • eagle
  • segfault
  • segmentation
  • command
  • eagle7
  • fault
  • line
  • cam
Related

Repeatable Segfault when running Eagle CAM generation from command line

Former Member
Former Member over 11 years ago

When I run any type of eagle command line CAM file generation I get a segmentation fault.

I'm running Linux Ubuntu 14.04.1 LTS and EAGLE Version 7.1.0 Copyright (c) 1988-2014 CadSoft.

The Eagle GUI seems to work fine.

 

Reproduction:

Breate board file in eagle and save as 'untitled.brd'

From command line run:

eagle -X -dGERBER_RS274X -ooutline.oln untiltled.brd Dimension

I always get the following output:

QPixmap: Cannot create a QPixmap when no GUI is being used

Segmentation fault (core dumped)

 

 

I've tried running Eagle in GDB and get the following traceback:

Program received signal SIGSEGV, Segmentation fault.

0x0862df42 in ?? ()

(gdb) bt

#0  0x0862df42 in ?? ()

#1  0x08627e4a in ?? ()

#2  0x08622b61 in ?? ()

#3  0x0825fced in ?? ()

#4  0x08229d4c in ?? ()

#5  0xf7929a83 in __libc_start_main () from /lib/i386-linux-gnu/libc.so.6

#6  0x0805a821 in ?? ()

 

I'm guessing the symbols are stripped, so the traceback might not be much use. I can generate and attach a core file if needed.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    This command works when running Eagle 5:

       eagle -X -dGERBER_RS274X -oexport.out  board.brd Top Bottom

       EAGLE Version 5.12.0 Copyright (c) 1988-2011 CadSoft                    

       CAM Processor: Gerber RS-274-X photoplotter, coordinate format 2.4 inch 

       finished.

     

    On the same system Eagle 7 still segfaults.  The system is running Ubuntu Linux 12.04.5 LTS

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    This command works when running Eagle 5:

       eagle -X -dGERBER_RS274X -oexport.out  board.brd Top Bottom

       EAGLE Version 5.12.0 Copyright (c) 1988-2011 CadSoft                    

       CAM Processor: Gerber RS-274-X photoplotter, coordinate format 2.4 inch 

       finished.

     

    On the same system Eagle 7 still segfaults.  The system is running Ubuntu Linux 12.04.5 LTS