EAGLE User Support (English) Repeatable Segfault when running Eagle CAM generation from command line
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
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 180 subscribers
  • Views 1166 views
  • Users 0 members are here
  • eagle
  • segfault
  • segmentation
  • command
  • eagle7
  • fault
  • line
  • cam
Related

Repeatable Segfault when running Eagle CAM generation from command line

Former Member
Former Member over 11 years ago

When I run any type of eagle command line CAM file generation I get a segmentation fault.

I'm running Linux Ubuntu 14.04.1 LTS and EAGLE Version 7.1.0 Copyright (c) 1988-2014 CadSoft.

The Eagle GUI seems to work fine.

 

Reproduction:

Breate board file in eagle and save as 'untitled.brd'

From command line run:

eagle -X -dGERBER_RS274X -ooutline.oln untiltled.brd Dimension

I always get the following output:

QPixmap: Cannot create a QPixmap when no GUI is being used

Segmentation fault (core dumped)

 

 

I've tried running Eagle in GDB and get the following traceback:

Program received signal SIGSEGV, Segmentation fault.

0x0862df42 in ?? ()

(gdb) bt

#0  0x0862df42 in ?? ()

#1  0x08627e4a in ?? ()

#2  0x08622b61 in ?? ()

#3  0x0825fced in ?? ()

#4  0x08229d4c in ?? ()

#5  0xf7929a83 in __libc_start_main () from /lib/i386-linux-gnu/libc.so.6

#6  0x0805a821 in ?? ()

 

I'm guessing the symbols are stripped, so the traceback might not be much use. I can generate and attach a core file if needed.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    Here's another data point.  I'm having a similar problem with CAM command lines on Windows 8.1 using Eagle 7.1.0, but not using Eagle 6.5.0.

    I'm seeing the problem using "-X d?".

     

    Trying:

    "C:\EAGLE-7.1.0\bin\eaglecon.exe" -X -d?

    returns error code -1073741819, which in hex is FFFFFFFFC0000005, when run from a Python script.

    If instead, run directly from a windows command prompt, Microsoft produces a popup that takes a minute to check for a fix, before prompting to close the program.

     

    Falling back to Eagle 6.5.0, it works OK with this command:

    "C:\Program Files (x86)\EAGLE-6.5.0\bin\eaglecon.exe" -X -d?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    On 10/9/2014 12:15 PM, Henry Forson wrote:

    Here's another data point.  I'm having a similar problem with CAM

    command lines on Windows 8.1 using Eagle 7.1.0, but not using Eagle

    6.5.0.

    I'm seeing the problem using "-X d?".

     

    Trying:

    "C:\EAGLE-7.1.0\bin\eaglecon.exe" -X -d?

    returns error code -1073741819, which in hex is FFFFFFFFC0000005, when

    run from a Python script.

    If instead, run directly from a windows command prompt, Microsoft

    produces a popup that takes a minute to check for a fix, before

    prompting to close the program.

     

    Falling back to Eagle 6.5.0, it works OK with this command:

    "C:\Program Files (x86)\EAGLE-6.5.0\bin\eaglecon.exe" -X -d?

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/128135

     

    This fix applies to 7.1.1 moving forward, so you have to test the

    command using 7.1.1. You can download 7.1.1 from our website

    www.cadsoftusa.com>Downloads>Betatest.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    I solved the problem calling eaglecon.exe ina first moment with the parameter -X-,  and then with the parameter -X+.

    Now my eaglecon callings generate correctly the gerbers file without open any brd visualization.

     

    By

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    I solved the problem calling eaglecon.exe ina first moment with the parameter -X-,  and then with the parameter -X+.

    Now my eaglecon callings generate correctly the gerbers file without open any brd visualization.

     

    By

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Running eagle with -X- -X+ fixes issue in 7.1.0, but seems to suppress text output while running (which isn't that much of a problem).

    Using eagle 7.1.1 BETA also fixes the issue.