EAGLE User Support (English) Centos 6 x86_64 Installation
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
  • State Not Answered
  • Replies 5 replies
  • Subscribers 178 subscribers
  • Views 554 views
  • Users 0 members are here
Related

Centos 6 x86_64 Installation

martynp
martynp over 11 years ago

Has anyone successfully installed Eagle on Centos???

 

The default repositories (and EPEL) don't have libssl.i686 or libcrypto.i686 - nor do they have openssl-libs.i686.

 

So any ideas?

 

I made the move from Windows to Linux at work, the FPGA tools are all working better than ever - but the only PCB design suite which works out of the box is Cadence and I would rather not have to change from Eagle...

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 10/10/14 20:23, Martyn Pittuck wrote:

    Has anyone successfully installed Eagle on Centos???

     

    No, but I'm running it on Fedora, also RPM-based

     

    The default repositories (and EPEL) don't have libssl.i686 or

    libcrypto.i686 - nor do they have openssl-libs.i686.

     

    So any ideas?

     

    Have you tried rpmfind? Or google? I typed "centos 6 libssl.i686" into

    google and got lots of hits with links to likely looking RPMs

     

    You will probably need to configure your system to have more than just

    the base repository set. This is almost universally true of RH-derived

    (and Debian-derived) distros. In fact the only one I've not had to do so

    on was Gentoo.

     

    HTH,

    Rob

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • martynp
    0 martynp over 11 years ago in reply to autodeskguest

    Yeah, I spent a couple of hours trying to get the dependencies installed, found the RPM's for Fedora but they use a newer version of glibc than is used in Centos 6.x - don't really fancy trying to change the glibc version, even if it is for the 32 bit libraries.

     

    However I did chase the dependency's to get the 32 bit glibc 2.17 installed, gave up when the list got passed 15 packages (was going to overwrite .so's which are used by the ARM cross compiler I'm using).

     

    I was hoping to either get a 'it works if you do this' or at least 'I eventually got there'.

     

    Thanks anyway!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to martynp

    On 10/10/2014 4:47 PM, Martyn Pittuck wrote:

    Yeah, I spent a couple of hours trying to get the dependencies

    installed, found the RPM's for Fedora but they use a newer version of

    glibc than is used in Centos 6.x - don't really fancy trying to change

    the glibc version, even if it is for the 32 bit libraries.

     

    However I did chase the dependency's to get the 32 bit glibc 2.17

    installed, gave up when the list got passed 15 packages (was going to

    overwrite .so's which are used by the ARM cross compiler I'm using).

     

    I was hoping to either get a 'it works if you do this' or at least 'I

    eventually got there'.

     

    Thanks anyway!

     

    Hi Martin,

     

    The key here is to setup a 32-bit environment under your 64-bit machine.

    I've attached a procedure that works under debian distros, it may take

    some tweaking to get it to work under an RPM based distro.

     

    hth,

    Jorge Garcia

     

     

     

    Attachments:
    Setting up a 32-bit environment in linux.txt.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • martynp
    0 martynp over 11 years ago in reply to autodeskguest

    Thanks for the info but I believe I am suck with the 32 bit environment I am using. The cross compiler uses pre-compiled binaries requiring one version of GLIBC and Eagle seems to require another.

     

    Anything other than the base yum repositories is going to be a difficult sell to the system admins.

     

    Time to look for alternatives, or use windows VM...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to martynp

    On 10/19/2014 12:23 PM, Martyn Pittuck wrote:

    Thanks for the info but I believe I am suck with the 32 bit environment

    I am using. The cross compiler uses pre-compiled binaries requiring one

    version of GLIBC and Eagle seems to require another.

     

    What 32-bit libraries do you have installed, and what libraries is Eagle

    expecting?

     

    Anything other than the base yum repositories is going to be a difficult

    sell to the system admins.

     

    The Linux linking loader will look for libraries in the directories

    listed in the environment variable "LD_LIBRARY_PATH" before it searches

    the standard locations. Once you locate the required shareable libraries

    you can put them in a directory separate from the system directories and

    point the loader at them.

     

    For example, I'm using Linux Mint 17 with Eagle 6.2.0 installed in /opt.

    It requires several libraries from older versions of the distribution.

    To see what libraries are missing, you can use the "ldd" command and

    look for the ones marked "not found". For example, on my system I'm

    missing libpng14.so.14:

     

      libXi.so.6 => /usr/lib/i386-linux-gnu/libXi.so.6 (0xf74e3000)

      libpng14.so.14 => not found

      libpthread.so.0 => /lib/i386-linux-gnu/libpthread.so.0 (0xf74c7000)

     

    I created a subdirectory /opt/eagle-6.2.0/lib and populated it with the

    shareable libraries I needed from an older system. When I invoke Eagle,

    I use this shell script, which handles defining LD_LIBRARY_PATH for me:

     

    #!/bin/bash

    EAGLE_DIR=/opt/eagle-6.2.0

    export LD_LIBRARY_PATH=$EAGLE_DIR/lib

    exec $EAGLE_DIR/bin/eagle

     

    Time to look for alternatives, or use windows VM...

     

    Nope, just time to learn more about Linux. Worst case you might have to

    compile a few libraries from source, but that'd be easier that

    reinstalling the whole set of libraries from Fedora.

     

    You'd need to post a list of the files you're missing before anyone is

    likely to be able to give you more help (unless Jorge decides to install

    a CentOS system to tinker with). Don't forget that CentOS is nothing

    more than RedHat Enterprise Linux recompiled with a different name. You

    may be able to find RHEL packages with what you need.

     

    -Reece