Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) High power class D Amp Build (5 channel, spectrum analyzer, pre&post-amp signal leveling)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 190 subscribers
  • Views 2000 views
  • Users 0 members are here
  • audio
  • high_performance
  • audio_engineering
  • amplifier
  • high_power
  • efficient
  • graphic_equalyzer
  • spectrum_analyzer
  • class_d
Related

High power class D Amp Build (5 channel, spectrum analyzer, pre&post-amp signal leveling)

e14 Contributor
e14 Contributor over 11 years ago

Well I hope this is the right place to start this discussion. I don't know much about element 14.

 

Anyways, to the point.

     The goal here is to make a high power (ie 5000w) 5 channel class d amp with signal leveling before and after the amplification process as well as having a spectrum analyzer. To get even more in depth when I explain this lets say I want it to take an audio signal in, analyze and level that signal, amplify that signal, analyze and level that signal again, send that signal to a spectrum analyzer, and cross that signal over to 5 channels (high-fq-l/r, mid-fq-l/r, and then 1 low-fq) all while maintaining great efficiency and audio quality.

     I need help making the power supply, the eq and spectrum analyzer (thinking about Arduino), the amp it self, and the cross-overs (everything pretty much). And It has to be from scratch (as much as possible).

 

     If I can get a list of all the components I need to have knowledge about I think I can figure out how to make this project come together. That's basically what I'm asking of you. Can Someone get me a list of components to research such as MOSFETS, Microprocessors, etc...?

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 11 years ago

    This isn't the right place so perhaps someone will move the thread to the audio group where it might be a better fit (it doesn't really have anything to do with Eagle).

     

    Having said that, I can't understand why you would want signal processing (of which leveling is just a special case) after the amplifier - you can't do complex digital signal processing on 5kW audio.

    Arduinos are no use here - you are into DSP territory.

     

    Building a kW level class D audio amplifier is quite an ambitious task - have you any experience of doing this sort of thing ?

     

    First you need to decide if you want to start on the signal processing side or the power amplifier side - then explain (to us and yourself) why you need 5kW which seems like far too much power (where are you going  to install this monster ?) . Once we know the power source and type of load it starts to be possible to define the design of the amplifier.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 11 years ago

    This isn't the right place so perhaps someone will move the thread to the audio group where it might be a better fit (it doesn't really have anything to do with Eagle).

     

    Having said that, I can't understand why you would want signal processing (of which leveling is just a special case) after the amplifier - you can't do complex digital signal processing on 5kW audio.

    Arduinos are no use here - you are into DSP territory.

     

    Building a kW level class D audio amplifier is quite an ambitious task - have you any experience of doing this sort of thing ?

     

    First you need to decide if you want to start on the signal processing side or the power amplifier side - then explain (to us and yourself) why you need 5kW which seems like far too much power (where are you going  to install this monster ?) . Once we know the power source and type of load it starts to be possible to define the design of the amplifier.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

         Well, the main goal is keeping the quality of the audio as good as possible. With that said, from what I understand there will be amounts of distortion after the amplification process. With another EQ, one would be able to get rid of some of that distortion... to my understanding at least.

         No I do not have any experience with this particular sort of thing, I am however in college for automation controls and SCADA, so I do have an understanding of what I might be getting into and I can get help along the way. I would have consulted my instructor but he does not get into this sort of thing.

         Anyways, this setup is going to be in a car, and eventually I want to be able to sell them. You see, I'm working on a prototype. I have a very large group of people I know who would love something like this and will pay big money for it. Besides that, my own passion and being an audiophile myself makes this all the more possible.

         The power source is going to be a bunch of battery's and hi-output- alternators much like what you would see in a professional sound competition set up or something like that. I'm not really worried to much about the power source entirely at the moment. Once I figure out what I need from the source to power all the components I want in this thing is when I'll work on it. to be honest I may decide to go up to 10kw. I'm dreaming big here I know but that's not going to stop me. haha.