EAGLE User Support (English) Symbols on Drills layer 44
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
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 181 subscribers
  • Views 451 views
  • Users 0 members are here
Related

Symbols on Drills layer 44

Former Member
Former Member over 11 years ago

Hi,

 

I am trying to place some very small feed-throughs between the pads on a BGA100 0.8 mm device.

 

I don't understand the white symbols shown on layer 44 on a board file for a feed through .

 

Using the Info button on a via, I can set the diameter to 0.485 and the drill to 0.25, which seems to fit well within the BGA pins.

 

The via is surrounded a white circle crossed by a white line at 45 degrees, both on layer 44.

 

What do the circle and line represent and where are their dimensions derived?

 

I assume that they are keep-out symbols but how can I change their values?

 

Thanks in advance for any help,

 

John.

  • Sign in to reply
  • Cancel
Parents
  • ingit
    0 ingit over 11 years ago

    "The via is surrounded a white circle crossed by a white line at 45 degrees, both on layer 44."\

    Those layers are drill and hole layer they simply show that here is a hole that needed to be drilled out.

    That lines will not affect anything. if it overlaps your BGA pin than also it will not affect. just a symbol not more than that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to ingit

    Hi,

     

    Thanks so much - that was a very helpful response.

     

    John.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to ingit

    Hi,

     

    Thanks so much - that was a very helpful response.

     

    John.