EAGLE User Support (English) Use ratsnest without having it physically fill polygon pours
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
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 178 subscribers
  • Views 734 views
  • Users 0 members are here
Related

Use ratsnest without having it physically fill polygon pours

Former Member
Former Member over 11 years ago

 

I am designing a 6layer board, using layers 2 and 5 as VDD and GND pours respectively.  Every time I hit ratsnest, it reduces airwires (for things connected to 2 and 5) but also fills the screen with copper.  It is very annoying trying to look through the copper to see traces below and above it.  I keep going to the edge of the board to move the polygon to lose the copper pour but not bring back the airwires (have done about a million times, very aggravating).  Is there a way to use ratsnest, have it reduce airwires (for things connected to pours), and not fill in the board?  If I turn off ratsnest processes polygons in Options/Set/Misc, it will not make any connections to either layer 2 or 5. Using EAGLE 6.5.0 professional.  Thanks. 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 11/11/2014 10:55 a.m., Nick S wrote:

     

    I am designing a 6layer board, using layers 2 and 5 as VDD and GND pours

    respectively.  Every time I hit ratsnest, it reduces airwires (for

    things connected to 2 and 5) but also fills the screen with copper.  It

    is very annoying trying to look through the copper to see traces below

    and above it.  I keep going to the edge of the board to move the polygon

    to lose the copper pour but not bring back the airwires (have done about

    a million times, very aggravating).  *Is there a way to use ratsnest,

    have it reduce airwires (for things connected to pours), and not fill in

    the board?*  If I turn off ratsnest processes polygons in

    Options/Set/Misc, it will not make any connections to either layer 2 or

    5. Using EAGLE 6.5.0 professional.  Thanks.

     

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/130837

     

     

    Does turning off those layers after a ratsnest not work for you?

     

     

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    Nick S wrote:

     

     

    I am designing a 6layer board, using layers 2 and 5 as VDD and GND pours

    respectively.  Every time I hit ratsnest, it reduces airwires (for

    things connected to 2 and 5) but also fills the screen with copper.  It

    is very annoying trying to look through the copper to see traces below

    and above it.  I keep going to the edge of the board to move the polygon

    to lose the copper pour but not bring back the airwires (have done about

    a million times, very aggravating).  *Is there a way to use ratsnest,

    have it reduce airwires (for things connected to pours), and not fill in

    the board?*  If I turn off ratsnest processes polygons in

    Options/Set/Misc, it will not make any connections to either layer 2 or

    5. Using EAGLE 6.5.0 professional.  Thanks. 

     

     

    there is 'ripup @' which removes the filling of all polygons

     

    or 'ripup @ signal-name(s)' with does the same but restricted to the

    listed signal(s)

     

     

    you could switch off your VDD & GND layers

     

     

    or perhapse hiding the airwires for VDD and GND (ratsnest ! GND VDD)

    will the job.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Brilliant! I should have thought of that a long time ago!