EAGLE User Support (English) Measuring distance between two objects
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
  • State Not Answered
  • Replies 7 replies
  • Subscribers 179 subscribers
  • Views 2679 views
  • Users 0 members are here
  • distance
  • measure
Related

Measuring distance between two objects

Former Member
Former Member over 11 years ago

Is there any way to measure edge-to-edge/center-to-center distance between two arbitrary objects? (like DesignSparkPCB)

  • Sign in to reply
  • Cancel
Parents
  • Joop14
    0 Joop14 over 11 years ago

    Use the mark command.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Joop14

    Measuring with MARK command requires very fine grid, right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to Former Member

    Normally parts have some datum, and edge or center is slightly meaningless - usually the part should be created with the datum at the most relevant place, because an outline often does not reflect the physical part in dimensions (and then an edge or center measurement will be in error).

    If the locations are needed for such edge-to-edge calculations, the datum should already be on the grid, so the MARK to snap to the grid is highly important for accurate measurements - otherwise if you have a need, you can go to a fine grid as you say, or you can press the Info button to get the exact location. Then you can refer to the part datasheet to identify where the edge of the component (to a tolerance) is with reference to the datum - this method would be more precise.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to shabaz

    image

    For example, I just want to measure distance between these two traces (a or b) "instantly".

    These are snapped to 0.1mm grid, but their edge is not on the grid.

    How can you do this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to Former Member

    For the top example, it is a math addition/subtraction. For the lower, I've never seen a need to do this for a PCB, but perhaps you do have a need. If it is a part, usually I would rotate the entire part (i.e. after it was created normally) - in that case, I would have checked the width if needed to, similar to the top example.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    On 2014-11-19 13:53:05 +0000, Naoya Yamada said:

    For example, I just want to measure distance between these two traces (a

    or b) "instantly".

    These are snapped to 0.1mm grid, but their edge is not on the grid.

    How can you do this?

     

    Most of my measurement needs between traces involve "how much space is

    between them?" so I flip to a 1mil grid and literally count squares. 

    The dimension/measure command is often too clunky because it's obsessed

    with snapping to some unknown point rather than using some simpler

    heuristic like "right here where I click, see that edge, that one!"

     

    -A.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    On 2014-11-19 13:53:05 +0000, Naoya Yamada said:

    For example, I just want to measure distance between these two traces (a

    or b) "instantly".

    These are snapped to 0.1mm grid, but their edge is not on the grid.

    How can you do this?

     

    Most of my measurement needs between traces involve "how much space is

    between them?" so I flip to a 1mil grid and literally count squares. 

    The dimension/measure command is often too clunky because it's obsessed

    with snapping to some unknown point rather than using some simpler

    heuristic like "right here where I click, see that edge, that one!"

     

    -A.