EAGLE User Support (English) Copy attributes across multiple sheets
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 180 subscribers
  • Views 797 views
  • Users 0 members are here
Related

Copy attributes across multiple sheets

bhodder
bhodder over 11 years ago

Hello,

 

I have a design which spans 17 sheets and need to change attributes on a part that has several copies across the sheets. I have tried to use both attrib-copy.ulp and attrib-add.ulp but they both continue to pop up "please select parts" even when parts are selected. Can anyone suggest a means of doing this without having to do it individual for each part?

 

Thanks,

Blake

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 11/26/2014 10:18 AM, Blake Hodder wrote:

    Hello,

     

    I have a design which spans 17 sheets and need to change attributes on a

    part that has several copies across the sheets. I have tried to use both

    attrib-copy.ulp and attrib-add.ulp but they both continue to pop up

    "please select parts" even when parts are selected. Can anyone suggest a

    means of doing this without having to do it individual for each part?

     

    Hi Blake,

     

    If the attributes are always going to be the same then it may be worth

    your while to set these in the libraries.

     

    Outside of the ULPs you've tried I'm not aware of any other solutions to

    this.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • coflynn
    0 coflynn over 10 years ago

    This is fixed just now in the latest attrib-add.ulp from GIT at https://github.com/robertstarr/ulp_user/blob/master/attrib-add.ulp . If enough time has passed since this posting it might be in the downloaded release too.

     

    (Note: I know the question is 1 year old... but this comes up as one of the first results when searching the topic so answered for anyone else stumbling upon this problem).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to coflynn

    Am 06.11.2015 um 22:16 schrieb Colin O'Flynn:

    This is fixed just now in the latest attrib-add.ulp from GIT at

    https://github.com/robertstarr/ulp_user/blob/master/attrib-add.ulp . If

    enough time has passed since this posting it might be in the downloaded

    release too.

     

     

    Many thanks. You should also change the version number and add

    an entry in the history.

     

    --

     

    Freundliche Grüße / Kind regards

    Friedrich

    -


    ... benutzen Sie nntp://news.cadsoft.de und einen

    funktionierenden News-Reader wie Thunderbird!

    ... use NNTP://news.cadsoft.de and a

    functional news reader like Thunderbird!

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • coflynn
    0 coflynn over 10 years ago in reply to autodeskguest

    Ah I'm not the author sorry! I just added a tiny fix to Bob Starr's awesome ULP collection, so didn't play with the versioning info.

     

    But I'm sure he'll be doing that at some point in the future.


    EDIT: I should also add, to use the atribs-add.ulp, you can use the select5.ulp in that same repository to form your selection/group. It will allow you to select components based on specific values etc and selects across all sheets. This lets you select all 100n capacitors in 0402 package size for example and give them an attribute with the specific part number.