EAGLE User Support (English) Unable to connect a net to VCC or GND
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 180 subscribers
  • Views 583 views
  • Users 0 members are here
Related

Unable to connect a net to VCC or GND

Former Member
Former Member over 11 years ago

Hello,

 

I'm new to Eagle CAD and have created a simple schematic. When I run the schematic, I get the warning:

Only 1 pin on net VCC

Only 1 pin on net VCC

The wires are connected to the pins because when I move the components (VCC and PINHD2x4), the wires stay connected. The grid has size 0.1 inch. Why do I get the warnings and how can I get rid of them? I've spent two days looking on forums and reading manuals, but haven't found a solution yet. I get the same error on other schematics if I connect any net to VCC or GND.

image

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    The warnings go away if I remove the VCC supply symbol, but I'm puzzled by this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 11/27/2014 1:02 AM, Radhika Grover wrote:

    Hello,

     

    I'm new to Eagle CAD and have created a simple schematic. When I run the

    schematic, I get the warning:

    Only 1 pin on net VCC

    Only 1 pin on net VCC

    The wires are connected to the pins because when I move the components

    (VCC and PINHD2x4), the wires stay connected. The grid has size 0.1

    inch. Why do I get the warnings and how can I get rid of them? I've

    spent two days looking on forums and reading manuals, but haven't found

    a solution yet. I get the same error on other schematics if I connect

    any net to VCC or GND.

     

    Hi Radhika,

     

    I hope you're doing well. EAGLE's basically telling you that there's

    only one connection to Vcc, at a bare minimum you need at least two

    connected points on a net.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nrv
    0 nrv over 11 years ago in reply to Former Member

    I had same problem few days ago...

    i think you have to close eagle, then re-open it...  Now, if you move component, you can see than Vcc is not connected anymore... delete old connection and make a new one...

    I hope that will solve your problem...

         nrv