EAGLE User Support (English) Handling of "Off-Board" Parts
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
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 529 views
  • Users 0 members are here
Related

Handling of "Off-Board" Parts

Former Member
Former Member over 11 years ago

How do I handle parts like a power switch or a meter which is on the drawing but not on the board? Do I need to draw two different drawings?

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    Gunther Hartung wrote:

    How do I handle parts like a power switch or a meter which is on the

    drawing but not on the board? Do I need to draw two different drawings?

     

     

    If you want to do it properly, yes. Because these parts are system

    components and not part of the PCB assembly. So they should not be on

    the schematic as components. If they are needed to understand the

    schematic you could draw them on another layer maybe.

     

    However, if they will be soldered to the board in the production process

    and then the boards with the external parts are one common assembly and

    stored in the warehouse as such then they should be drawn on the

    schematic. Like the OLED display on this board, it's flopping about but

    soldered to the board and thus part of board:

     

    https://cdn.sparkfun.com//assets/parts/9/9/5/6/13003-01.jpg

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer