EAGLE User Support (English) ULP that works in either Schematic or Board?
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 179 subscribers
  • Views 256 views
  • Users 0 members are here
Related

ULP that works in either Schematic or Board?

Former Member
Former Member over 11 years ago

I'd like some of my ULPs that do useful stuff like lining up objects and globally changing type to work in either schematic or board.

 

1) Can you point me to a ULP that works in either schematic or board?

2) Is the easiest way to implement this basically to duplicate the ULP for both board and schematic, then send the program to the appropriate code for schematic or board?

3) Along the same lines, is there any higher abstraction in which one could refer to either schematic or board?

 

thanks,

 

Paul

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

     

    "hbridge77"  skrev i nyhetsmeldingen:

    855287547.131419272573250.JavaMail.jive@flmspu-csapp-02.premierfarnell.com

    ...

     

    I'd like some of my ULPs that do useful stuff like lining up objects and

    globally changing type to work in either schematic or board.

     

    Use the loop members

    project.board(B)

    and

    project.schematics(S)

     

    Remember changing anything needs to be done via a script that you may return

    with exit(commandstring)