EAGLE User Support (English) Aligning Text to be read from the Left
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 181 subscribers
  • Views 542 views
  • Users 0 members are here
  • alignment
  • text
Related

Aligning Text to be read from the Left

sailmike1
sailmike1 over 11 years ago

I'm making a prototyping board for 4 different types of LED's on one board. I need to align some of the text so it can be read from the left side and top of the board. Rotating the text doesn't work because the text can only be read from either the bottom or right side of the board. The text I'm trying to align to be read from the left is circled in the photo. How do I align the text?

 

Thanks,

Mikeimage

  • Sign in to reply
  • Cancel
Parents
  • sailmike1
    0 sailmike1 over 11 years ago

    Someone on another forum explained that the upside down ABC+ icon can be use to reorient the text to the direction I wanted and that works. I would first click on the text icon, enter the text, rotate the text to the side I want it readable from, then click on the upside down ABC+ icon to flip it. Seems like a lot of steps just to get the text into the orientation I want.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • sailmike1
    0 sailmike1 over 11 years ago

    Someone on another forum explained that the upside down ABC+ icon can be use to reorient the text to the direction I wanted and that works. I would first click on the text icon, enter the text, rotate the text to the side I want it readable from, then click on the upside down ABC+ icon to flip it. Seems like a lot of steps just to get the text into the orientation I want.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Richard_H
    0 Richard_H over 11 years ago in reply to sailmike1

    Michael,

     

    the workflow could look like this.

     

    Click the Text icon

    Type the text + OK

    Now the text is following the mouse cursor

    Click the "spin" icon in the parameter toolbar

    Type in the angle + enter

    Place it.

     

    Once done the this parameters are used for the next text (which is already following the mouse cursor)

    Type in new text and place it

     

    Not so complicated, I guess..

     

    BR

    Richard