EAGLE User Support (English) Eagle: assigning 2 names to one net
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
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 181 subscribers
  • Views 2825 views
  • Users 0 members are here
Related

Eagle: assigning 2 names to one net

Former Member
Former Member over 11 years ago

I have a schematic where I've created and named a net for each pin on a controller.  I now want to tie one of those pins ("enable") to ground, but I don't want the name of the net to change to "GND", it needs to stay "enable".

 

Can you please tell me how to assign two names into one net? (without putting a 0R resistor between the two :-) )

 

Thanks,

 

DougM

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 11 years ago

    On 02/03/2015 02:13 PM, doug metzler wrote:

    I have a schematic where I've created and named a net for each pin on a

    controller.  I now want to tie one of those pins ("enable") to ground,

    but I don't want the name of the net to change to "GND", it needs to

    stay "enable".

     

    Can you please tell me how to combine two names into one net? (without

    putting a 0R resistor between the two image )

     

    Well... you can't.  But there is a workaround to accomplish your goal.

    Use a short from the shorts library.  The symbol is essentially two pins

    connected to each other, and the package is overlapping pads.  This

    generates an overlap DRC error which can be safely approved.

     

    Wire one side of the short to your controller, and the other side to ground.

     

    This method is often used to connect multiple grounds (DGND, AGND, GND2,

    etc) to a single ground (GND) potential.  There's plenty of threads in

    this forum about connecting two grounds.

     

    There is a thread about this titled "Merging nets" that was started on

    03-Apr-2011. You can download a SHORTS library from Olin Lathrop at

    http://www.embedinc.com/pic/dload.htm.  I took Olin's library and added

    a few packages to it myself on an as-needed basis.

     

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • dukepro
    0 dukepro over 11 years ago

    On 02/03/2015 02:13 PM, doug metzler wrote:

    I have a schematic where I've created and named a net for each pin on a

    controller.  I now want to tie one of those pins ("enable") to ground,

    but I don't want the name of the net to change to "GND", it needs to

    stay "enable".

     

    Can you please tell me how to combine two names into one net? (without

    putting a 0R resistor between the two image )

     

    Well... you can't.  But there is a workaround to accomplish your goal.

    Use a short from the shorts library.  The symbol is essentially two pins

    connected to each other, and the package is overlapping pads.  This

    generates an overlap DRC error which can be safely approved.

     

    Wire one side of the short to your controller, and the other side to ground.

     

    This method is often used to connect multiple grounds (DGND, AGND, GND2,

    etc) to a single ground (GND) potential.  There's plenty of threads in

    this forum about connecting two grounds.

     

    There is a thread about this titled "Merging nets" that was started on

    03-Apr-2011. You can download a SHORTS library from Olin Lathrop at

    http://www.embedinc.com/pic/dload.htm.  I took Olin's library and added

    a few packages to it myself on an as-needed basis.

     

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer