Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Battery and nRF24L01 connections and definitions in Eagle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 2433 views
  • Users 0 members are here
  • nrf24l01+
  • connection
  • battery
  • solderability
Related

Battery and nRF24L01 connections and definitions in Eagle

e14 Contributor
e14 Contributor over 11 years ago

Hello,

 

I am designing a board that has 4 sensors and an nRF24L01 wireless module to send the sensor readings off to a base station.  It's quite similar to maniacbug's Low Power Sensor project.  I'm doing a thru-hole design.

 

I'm a new Eagle user, but think I am coming up to speed pretty reasonably with some of the very good tutorials on YouTube and looking at other projects for examples.  I have a few random questions.

 

1.  For powering my project, I am thinking of using 2 AAA or 2 AA batteries, putting them in a separate holder and just soldering power leads to the board.  So in Eagle schematic, how would I define these solder points in the schematic and the board layout?

 

2.  The nRF24L01 wireless module  that I have is a separate breakout board that has a block of 2x4 long, square header pins.  Hopefully you can see the image below.  What is the best way to connect this to the main board?  Pins look a bit big to solder.  I've looked around at female sockets to mount on the main board, but I'm not convinced I have found the right solution.  Any suggestions?

transceiver-nrf24l01-module.jpg

 

Thanks for any suggestions,

   Steve

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 02/08/2015 09:14 PM, Steve McCrew wrote:

    Hello,

     

    I am designing a board that has 4 sensors and an nRF24L01 wireless

    module to send the sensor readings off to a base station.  It's quite

    similar to maniacbug's Low Power Sensor

    (https://maniacbug.wordpress.com/2011/10/19/sensor-node/) project.  I'm

    doing a thru-hole design.

     

    I'm a new Eagle user, but think I am coming up to speed pretty

    reasonably with some of the very good tutorials on YouTube and looking

    at other projects for examples.  I have a few random questions.

     

    1.  For powering my project, I am thinking of using 2 AAA or 2 AA

    batteries, putting them in a separate holder and just soldering power

    leads to the board.  So in Eagle schematic, how would I define these

    solder points in the schematic and the board layout?

     

    2.  The nRF24L01 wireless module  that I have is a separate breakout

    board that has a block of 2x4 long, square header pins.  Hopefully you

    can see the image below.  What is the best way to connect this to the

    main board?  Pins look a bit big to solder.  I've looked around at

    female sockets to mount on the main board, but I'm not convinced I have

    found the right solution.  Any suggestions?

     

     

    To provide pads for connecting your battery holder, you might want to

    look at the "PINHD-1x1" or "PINHD-1x2" devices in the "pinhead" library.

    They're intended for use with pin header strips, but they'd probably

    work with the wires on your battery holder. Check the diameter of the

    wire vs the finished diameter of the hole.

     

    I built something very similar a while back, also using the nRF24L01+

    module. You can get female sockets that will accept a pin header like

    that on the module, but unless you absolutely have to be able to remove

    the module you'd probably be better off using a PINHD-2x4 device to lay

    out your board. After inserting the module pins through your PCB, clip

    them off short before soldering them in place.

     

    Bear in mind that the PCB traces on the module on the other end from the

    connector forms an antenna. It won't behave properly if you mount

    components, route traces, or place a ground plane under it. Best to let

    about half the module extend beyond the end of your PCB, or at worst

    have a large area of totally bare board (no components, no copper) near it.

     

    Another thought is to watch the discharge curves for standard Alkaline

    batteries. They start above the nominal 1.5V, then head south at a

    pretty fair clip. At full discharge they put out barely 0.9V each. The

    nRF24L01+ is rated from 3.6V to 1.9V, but the microprocessor you use may

    not be happy. I used a PIC 16LF876 in my initial design because it's

    rated to run down to 2.0V.

     

    -Reece

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    Thanks for sharing your experience.  This is very helpful to me.

     

    -Steve M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    Thanks for sharing your experience.  This is very helpful to me.

     

    -Steve M.