EAGLE User Support (English) Adding attribute name and value to symbol
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 179 subscribers
  • Views 583 views
  • Users 0 members are here
Related

Adding attribute name and value to symbol

Former Member
Former Member over 11 years ago

I'm defining an part device for an LED.  The LED Device has an attribute called "BRIGHTNESS".  When I add the device to a schematic, I would the attribute to be shown by default, along with it's value (e.g, "BRIGHTNESS = 90").

 

If I added a text item with ">BRIGHTNESS" to the symbol, the value will appear alone by default in the schematic (e.g. "90"). 

 

On the other hand, if I use the attribute tool, I can make the it show up as "BRIGHTNESS = 90" by selecting the "both" from the display menu.

 

Is there a way to get the "display both" behavior automatically by setting something in the symbol?

 

-steve

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 13/02/2015 7:06 p.m., Steven Swanson wrote:

    I'm defining an part device for an LED.  The LED Device has an attribute

    called "BRIGHTNESS".  When I add the device to a schematic, I would the

    attribute to be shown by default, along with it's value (e.g,

    "BRIGHTNESS = 90").

     

    If I added a text item with ">BRIGHTNESS" to the symbol, the value will

    appear alone by default in the schematic (e.g. "90").

     

    On the other hand, if I use the attribute tool, I can make the it show

    up as "BRIGHTNESS = 90" by selecting the "both" from the display menu.

     

    Is there a way to get the "display both" behavior automatically by

    setting something in the symbol?

     

    -steve

     

    As it says in the HELP > Editor Commands > TEXT >attributes

     

    If you define in the symbol a text object >BRIGHTNESS=

    Then in the device an attribute BRIGHTNESS with a value of, say, 50

    When added to the schematic the part will display a text saying

    BRIGHTNESS = 50

     

    HTH

    Warren