Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Iterface IC 555 Project To Laptop or PC
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 191 subscribers
  • Views 1692 views
  • Users 0 members are here
  • eagle
  • schematic
  • question
Related

Iterface IC 555 Project To Laptop or PC

e14 Contributor
e14 Contributor over 11 years ago

Hello,
How are you doing today?
I am a student of electronics, information technology and mathematics. I need to develop a way o display the IC 555 (astable mode o monostable mode) on and off to a laptop or a desktop. I need to show the accuracy of the RC time constant, or show the percentage difference between the formula and actual numbers being displayed...

 

Do you have ANY suggestions.


Let me know.

 

I look forward to hearing from you...

 

 


Thank you,

 

 

Charles L. Phillips

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    If you look at 555 Timer , you will see a good analysis of the chip. A LED can be used to see when the chip can pulse. If you need to do with a laptop, check out arduino using serial interface.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to clem57

    Let me google that for you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago in reply to clem57

    Let me google that for you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • gpsmikey
    0 gpsmikey over 11 years ago in reply to gadget.iom

    To accurately measure the time periods of the 555 circuit, you need an

    accurate measurement device.  One such potential device would be an Arduino

    (you can get a small Arduino board very reasonably priced).  You would have

    to connect it to your test circuit and write code for the Arduino board to

    monitor the output of the 555 (make sure you are using the same voltages on

    everything or you will have to address the issue of voltage level

    translation).  The Arduino would monitor the status and send that

    information to the laptop.  While a laptop with a parallel interface could,

    in theory, monitor the output of your 555 using one of the input lines on

    the interface, it would be very difficult since the OS on the laptop is

    busy doing multiple tasks so timing is very tough.  There are a number of

    sites dedicated to working with Arduino boards and creating "sketches"

    (their name for programs).  Another option is simply use a decent

    oscilloscope and measure the times that way, entering the information by

    hand into your table.  Depends on the accuracy needed - you don't mention

    just what your definition of "accuracy" is - 5%?, 1%? 1us?

     

    mikey

     

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to clem57

    clem57

     

    From what I've determind his issue isn't with making the 555 timer, but with electronically measuring the pulse frequency his circuits are generating.