EAGLE User Support (English) can't connect to middle of arc
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 280 views
  • Users 0 members are here
Related

can't connect to middle of arc

rickford66
rickford66 over 10 years ago

Running Eagle 6.5.0.

Is there a way to force a connection to the middle of an arc, or do I have to split the arc in two and make the connection where the two arcs join?

Thanks.

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    Am 02.03.2015 um 16:12 schrieb rickford66:

    Running Eagle 6.5.0.

    Is there a way to force a connection to the middle of an arc, or do I

    have to split the arc in two and make the connection where the two arcs

    join?

    Thanks.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/142201

     

     

    An arc is responsive at its ends only. You have to combine e.g.

    two arcs.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/