EAGLE User Support (English) Logical Operations on Artwork
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 179 subscribers
  • Views 411 views
  • Users 0 members are here
Related

Logical Operations on Artwork

Former Member
Former Member over 10 years ago

Hello Eagle community, wondering if there is a clever way to do logical operations on artwork, e.g. I'd like to create an annulus by removing part of a circle? Thank you.Logical

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 10 years ago

    On 03/06/2015 10:53 AM, John Sevic wrote:

    Hello Eagle community, wondering if there is a clever way to do logical

    operations on artwork, e.g. I'd like to create an annulus by removing

    part of a circle? Thank you.Logical

     

    I believe you can do it on the top or bottom copper layers, but not any

    inner layers.

     

    Try adding a circle to the top copper layer for the outer diameter.

    Then add a circle for the inner diameter on the tRestrict layer.  You

    could do this in the package editor in a library and treat the ring as a

    device that could be translated or mirrored to the bottom.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to dukepro

    Chuck, thanks, What I am trying to is create a circular ground-plane for a monopole antenna, with the feed coming in through the top metal also. So, I need the keep-out to be in the center of the ground-plane for the monopole soldering hole, as well as keep-out for the (microstrip) trace. From your suggestion, using the tRestrict layer, does that instruct Eagle to not place metal in the shape of the object on tRestrict, or do I need to merge these layers?

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to dukepro

    Chuck, thanks, What I am trying to is create a circular ground-plane for a monopole antenna, with the feed coming in through the top metal also. So, I need the keep-out to be in the center of the ground-plane for the monopole soldering hole, as well as keep-out for the (microstrip) trace. From your suggestion, using the tRestrict layer, does that instruct Eagle to not place metal in the shape of the object on tRestrict, or do I need to merge these layers?

     

    Thanks.