EAGLE User Support (English) View Only Mode
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 180 subscribers
  • Views 292 views
  • Users 0 members are here
Related

View Only Mode

JasonTraud
JasonTraud over 10 years ago

What about a View Only mode or a lock-out feature where the only tools able to be used are the Show and Inspect tools. This would be great for firmware guys to jump in and verify the port connections without running the risk of accidentally making a change and saving. Or for a technician to pop in when assembling a prototype or setting up a pick and place machine.

 

It wouldn't even need to be a modification to the existing editor but a seperate viewer program that is only capable of viewing the schematic and board in a stripped down and clean interface.

  • Sign in to reply
  • Cancel

Top Replies

  • Joop14
    Joop14 over 10 years ago +1
    There's no need to. On a network, when you are the owner of the files, make sure that only you have write-access to the files. This way they can follow the latest changes but they can not change anything…
  • Joop14
    0 Joop14 over 10 years ago

    There's no need to. On a network, when you are the owner of the files, make sure that only you have write-access to the files. This way they can follow the latest changes but they can not change anything.

    If you send them a copy of your files instead, tell them to change the fileproperties to read-only.