EAGLE User Support (English) Is there anyway to exclude parts from the PCB
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
  • State Not Answered
  • Replies 29 replies
  • Subscribers 181 subscribers
  • Views 4463 views
  • Users 0 members are here
Related

Is there anyway to exclude parts from the PCB

Former Member
Former Member over 11 years ago

In Eagle Cad, is there anyway to exclude components on the schematic from the board view? I have several parts that will be wired to screw terminals. They still need to be shown in the schematic, but I do not need or want them on the board. I can't leave them outside the board area, so what's a guy to do? Thanks...

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 11 years ago +1
    On 3/26/2015 4:38 AM, Derek Tombrello wrote: In Eagle Cad, is there anyway to exclude components on the schematic from the board view? I have several parts that will be wired to screw terminals. They still…
  • autodeskguest
    autodeskguest over 9 years ago in reply to Former Member +1
    Mark Winters wrote: Hello Jorge. I wonder if you could point me to some documentation that helps me to remove the package as explained. I have made a copy of the component in my own library but return…
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 3/26/2015 4:38 AM, Derek Tombrello wrote:

    In Eagle Cad, is there anyway to exclude components on the schematic

    from the board view? I have several parts that will be wired to screw

    terminals. They still need to be shown in the schematic, but I do not

    need or want them on the board. I can't leave them outside the board

    area, so what's a guy to do? Thanks...

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/145238

     

     

    Hi Derek,

     

    I hope you're doing well. This is possible. In the library for those

    components create an attribute with the name EXTERNAL. This tells

    EAGLE that this part is off board and therefore doesn't require a

    package on the board layout.

     

    In order for this to work the device can not have a package. So you may

    need to create a variant of those parts without packages.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 3/26/2015 4:38 AM, Derek Tombrello wrote:

    In Eagle Cad, is there anyway to exclude components on the schematic

    from the board view? I have several parts that will be wired to screw

    terminals. They still need to be shown in the schematic, but I do not

    need or want them on the board. I can't leave them outside the board

    area, so what's a guy to do? Thanks...

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/145238

     

     

    Hi Derek,

     

    I hope you're doing well. This is possible. In the library for those

    components create an attribute with the name EXTERNAL. This tells

    EAGLE that this part is off board and therefore doesn't require a

    package on the board layout.

     

    In order for this to work the device can not have a package. So you may

    need to create a variant of those parts without packages.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 9 years ago in reply to autodeskguest

    Hello Jorge. I wonder if you could point me to some documentation that helps me to remove the package as explained. I have made a copy of the component in my own library but return an error when I try to remove its package. ????

     

    image

     

    I am a complete novice but Im into it.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to Former Member

    Mark Winters wrote:

     

    Hello Jorge. I wonder if you could point me to some documentation that

    helps me to remove the package as explained. I have made a copy of the

    component in my own library but return an error when I try to remove

    its package. ????

     

     

    I am a complete novice but Im into it.....

     

     

    posting a totally unrelated question into a old tread from april 2015

    won't do you any good.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to Former Member

    On 7/22/2016 4:47 AM, Mark Winters wrote:

    Hello Jorge. I wonder if you could point me to some documentation that helps me to remove the package as explained. I have made a copy of the component in my own library but return an error when I try to remove its package. ????

     

     

    I am a complete novice but Im into it.....

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/202074

     

     

    Hi Mark,

     

    I hope you're doing well. As Lorenz has pointed out, it's best to start

    a new thread when you have a new question. However, I know Element14

    doesn't make that easy for new users. In the future it might be easier

    for you to use the forum mirror here:

     

    http://eaglecentral.ca/

     

    Now on to your problem. EAGLE will not let you delete a package if it is

    associated with a device. So the first thing you have to do it open the

    device that uses that package. Remove the package from the device by

    first clicking on the connect button at the bottom right of the device

    editor. Undo all of the connections. Then you'll be able to delete the

    package from the device and ultimately from the library if you so wish.

     

    hth,

    Jorge Garcia