EAGLE User Support (English) how to define non-signal (ground) layer in v7.2
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
  • State Verified Answer
  • Replies 25 replies
  • Subscribers 181 subscribers
  • Views 4509 views
  • Users 0 members are here
  • signal
  • 7.2
  • plane
  • non
  • ground
  • layer
Related

how to define non-signal (ground) layer in v7.2

Former Member
Former Member over 10 years ago

Using the standard version, with a top/bottom and 3 other routing inner layers, a very split power plane layer, how do I define a non-signal inner ground layer that can be polygon poured and get anti-pads around non-ground signal vias during ratsnest?

Stackup will be with only 6 signal layers (if you count the power plane):

1) Top with SMT, low frequency traces, and some high speed routing traces

2) desired inner ground layer

3) inner low frequency routing layer

4) Power plane

5) a 2nd copy of the inner ground layer

6) inner high frequency routing layer

7) inner high frequency routing layer

8) Bottom with SMT components...

Note that I'm going to be using TH vias rather than buried or blind vias, as well as some TH connectors

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 10 years ago

    Eagle advertises 6 signal layers in standard version.  How do I define non-signal board layer?

    Anyone willing to answer?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    Hi Bruce,

     

    In the display command you can click the ADD button to add non-signal

    layers.

     

    It can also be done from the command line with the LAYER command.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    Hi Bruce,

    In the display command you can click the ADD button to add non-signal
    layers.

    It can also be done from the command line with the LAYER command.

    Let me know if there's anything else I can do for you.

    Best Regards,
    Jorge Garcia

    Thank you Jorge. Posted here from official Eagle site.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Jorge,

    in 7.2 do you mean the NEW button in the display window?

    Once the layer is defined as layer 100, I pour a polygon, have a via go through it with a non-ground signal, and  ratsnest, I don't see an anti-pad created around the capture pad.

    In the original question.....how do I define a non-signal inner ground [board] layer that can be polygon poured and get anti-pads around non-ground signal vias during ratsnest?

    Correspondingly, I trying to define the layer 100 in DesignRules and it will not let me define layer 100 in the board.

    I still can't seem to define a non-signal inner board layer that ratsnests.  I need this non-signal layer as well as the 6 signal layers in the original question.

    What am I missing?

    ...Bruce

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    On 22/04/15 21:31, Bruce Mellen wrote:

    In the original question.....how do I define a non-signal inner ground

    layer that can be polygon poured and get anti-pads around

    non-ground signal vias during ratsnest?

     

    The problem is your incorrect terminology. When you say "non-signal" you

    don't mean that. Ground is a signal (net) just like any other. What you

    want is a "supply layer".

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to clem57

    Clem Martins wrote on Thu, 23 April 2015 05:37

    Hi Bruce,

     

    In the display command you can click the ADD button to add

    non-signal

     

      layers.

     

      It can also be done from the command line with the LAYER

    command.

     

      Let me know if there's anything else I can do for you.

     

      Best Regards,

      Jorge Garcia

    Thank you Jorge. Posted here from official Eagle site.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/147827

     

     

     

    From where?

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    I see supply layer listed nowhere in the 7.2 HELP.  I thought I heard it was to be phased out.  What has taken its place?  I have 6 layers I need to route but additionally need a couple ground planes in the middle of the stackup, as supposedly could be done in older versions.  The planes just need to accept pours and get antipads around TH vias when ratsnest.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    On 04/24/2015 10:10 PM, Bruce Mellen wrote:

    I see supply layer listed nowhere in the 7.2 HELP.  I thought I heard it

    was to be phased out.  What has taken its place?  I have 6 layers I need

    to route but additionally need a couple ground planes in the middle of

    the stackup, as supposedly could be done in older versions.  The planes

    just need to accept pours and get antipads around TH vias when ratsnest.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/148154

     

    Just use a named polygon over the layer to replace the old style power

    plane. It will clear via and routes if you need to use that layer for

    short distances.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    Polygon on what layer number? I tried that on a layer numbered 100 or higher, but it did not create the anti-pads/clearance for the TH vias already on the signal layers, as it does not allow a signal name to be entered for the polygon.  I'm already using all 6 signal layers for routing and need a separate dedicated ground/supply plane that just accepts polygons and has clearance around the vias when doing a ratsnest.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    Bruce Mellen wrote on Thu, 30 April 2015 14:39

    Polygon on what layer number? I tried that on a layer numbered 100 or

    higher, but it did not create the anti-pads/clearance for the TH vias

    already on the signal layers, as it does not allow a signal name to be

    entered for the polygon.  I'm already using all 6 signal layers for

    routing and need a separate dedicated ground/supply plane that just

    accepts polygons and has clearance around the vias when doing a

    ratsnest.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/148450

     

     

    Hi Bruce

     

    Your thread subject is a contradiction. A ground layer is a signal layer.

    i.e. the signal name is "ground".

     

    Your version has 6 copper layers which equates to 6 signal layers. You

    cannot create any more signal layers.

    What you can create is a user defined layer. These are not signal layers

    and do not work like the  signal layers, with all the magic like polygons

    keeping away from other signals and the auto router ignoring other signals,

    for example.  No magic occurs as they are simply drawing layers like the

    documentation layers. You define them above layer 99.

     

    So you will need to find another way to do what you want.

     

    Is what you are after, another copy of layer 2 or 5? If so ,you could use

    the ULP copy-layer-to-any-layer.ulp to copy the polygon wires to another

    non signal layer and include that layer as another Gerber file (layer). You

    will need to address the via restrings on that layer also.

     

     

    HTH

    Warren

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>