EAGLE User Support (English) use library
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
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 327 views
  • Users 0 members are here
  • library
Related

use library

xeptio
xeptio over 10 years ago

Hello ,

 

I have a problem on eagle 7.2 , I created my library of the PK70FN1M0VMJ12 , with pads of 0.4mm of diameter and with 0.25mm drills, but when I use this library in a board the diameter of the pads change , could you say me why? and how I can do to repair that ?

 

Thanks

 

MD

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 10 years ago

    Am 14.04.2015 um 11:51 schrieb m d:

    Hello ,

     

    I have a problem on eagle 7.2 , I created my library of the

    PK70FN1M0VMJ12 , with pads of 0.4mm of diameter and with 0.25mm drills,

    but when I use this library in a board the diameter of the pads change ,

    could you say me why? and how I can do to repair that ?

     

    Set the following paramter to 0:

     

    DRC

    card Resting

     

               Min     %     Max       Diameter

     

    Top        0mm    0     0.508mm

     

    Inner      0mm    0     0.508mm  

     

    Bottom     0mm    0     0.508mm

     

    Read also ...\doc\manual_en.pdf

    page 153 - 155

    Chapter: 6.3 Considerations Prior to Creating a Board

     

     

     

    ***

    Um das Original zu lesen, und auch zuverlässig angehängte Dateien

    bereitstellen zu können, benutzen Sie news.cadsoft.de und einen

    funktionierenden News-Reader wie Thunderbird!

    ***

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    ______________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschaeftsfuehrer: Mark Whiteling

    ______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • xeptio
    0 xeptio over 10 years ago in reply to Former Member

    thanks that's work