EAGLE User Support (English) move part of component to new sheet
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
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 509 views
  • Users 0 members are here
Related

move part of component to new sheet

Former Member
Former Member over 10 years ago

I have a component, lets say a "G2R" relay from the standard "relay.lbr". Can I put the Coil on one sheet and the contacts on another? If so, how?  Oh, I am using Eagle 7.2.0.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 14/04/15 20:15, Chris Boland wrote:

    I have a component, lets say a "G2R" relay from the standard

    "relay.lbr". Can I put the Coil on one sheet and the contacts on

    another? If so, how?  Oh, I am using Eagle 7.2.0.

     

    Yes, no problem. There are two ways:

     

    As you're using a recent version, you will have a column of thumbnails

    of pages down the left side. Place your relay (both parts) on one sheet,

    say the one you want the coil on, using the "ADD" dialog. Then "move"

    the part you want elsewhere (in this case the contacts) and drag it

    across to the thumbnail of the sheet you want it to be on.

     

    Alternatively you can still use the old way. Using "ADD", place only the

    coil on the sheet where you want it. If you get both parts at once,

    delete the contacts. Make a note of the part number, e.g. RL1. Select

    the sheet where you want the contacts and enter the command "invoke

    RL1". You will be offered a list of all the remaining bits (the

    contacts) and you can place them as you normally would.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    The first option doesn't work (for me anyway), the second option did what I wanted.

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    The first option doesn't work (for me anyway), the second option did what I wanted.

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    On 14/04/15 22:37, Chris Boland wrote:

    The first option doesn't work (for me anyway),

     

    Oh! Well, I may have got some details wrong as the license I have is for

    V4 so the "new way" is not something I've actually used.

     

    the second option did

    what I wanted.

    Thanks!

     

    You're welcome.