EAGLE User Support (English) Board dimensions in free version
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 180 subscribers
  • Views 424 views
  • Users 0 members are here
Related

Board dimensions in free version

Former Member
Former Member over 10 years ago

Is it possible to create a 3.2x4 board instead of a 4x3.2 board in the free version of Eagle?  I've tried rotating the board but I still get the "free version can't" ... error.  There's an old answer on this forum from 2010 saying it should work but I'm not sure if that's the still the case.

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago in reply to clem57 +1
    Clem Martins wrote: Why not rotate the components instead of the board... Clem I think that's what was being suggested in the first answer.
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 22/04/15 20:57, Walid Hosseini wrote:

    Is it possible to create a 3.2x4 board instead of a 4x3.2 board in the

    free version of Eagle?  I've tried rotating the board but I still get

    the "free version can't" ... error.  There's an old answer on this forum

    from 2010 saying it should work but I'm not sure if that's the still the

    case.

     

    No. The freeware limitation is very clearly defined in terms of maximum

    values for X and Y coordinates. You cannot swap them.

     

    However, there is nothing to stop you designing your board in

    "landscape" even if your final fitment will be "portrait". You will need

    to be careful about rotating an existing design (whether partial or

    created in a paid-for version) because any placement outside the 4x3 box

    will be an error.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    Why not rotate the components instead of the board...

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to clem57

    Clem Martins wrote:

     

    Why not rotate the components instead of the board...

    Clem

    I think that's what was being suggested in the first answer. image