EAGLE User Support (English) Hide Components on Layers
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
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 180 subscribers
  • Views 1795 views
  • Users 0 members are here
  • placement
  • eaglecad
  • pcb
  • component
  • layers
Related

Hide Components on Layers

oldmanraskers
oldmanraskers over 10 years ago

Hi,

I'm putting components on both sides of a dual layer board, the problem is that the components are all overlapped and I cant really see what is happening - so I wonder if there is a way to hide the components on the bottom layers whilst I work on the top layer placement and vice versa?

Regards, oldmanraskers

  • Sign in to reply
  • Cancel

Top Replies

  • kikoun
    kikoun over 10 years ago +1 verified
    Hi, The easy way is to have a shortcut to hide bplace(22), borigin(24) and bdocu(52) layers, to display them, and same for top (tplace(21), borigin(23) and bdocu(51) layers). to do that, you go on 'option…
  • kikoun
    0 kikoun over 10 years ago

    Hi,

     

    The easy way is to have a shortcut to hide bplace(22), borigin(24) and bdocu(52) layers, to display them, and same for top (tplace(21), borigin(23) and bdocu(51) layers).

     

    to do that, you go on 'option>assign' menu and you can assign key, to different display option:

    F1 will display top layer, and tplace, torigin and tkeepout, while Crtl+F1 will hide them.

    the shift version "Shift F1" and "shift ctrl F1"  do the same but whit the tdocu.

     

    F4 is for the bottom...

     

    At first I was using different key and I alway mix up every thing... so I tried to organize my shortcut in a way that is easier to remember (for me, you should found your own organization ). I give you my organization as an simple example: 

     

    Ctrl + Fx : hide layers

    no Ctrl + Fx : display

     

    F1 to F4 : Main routing layer from top to bottom (F1 top, F4 bottom)

    Shift+Fx : additional layers that I use less like F1= tdocu, F2=GND plane on 2nd routing layer, .....

     

    If I work on 6 layer's PCB this will be :

    F1 > Top route layer

    Shift + F1 : Part tdocu layer.

    Shift + F2  : Second route layer (usually a GND  plane)

    F2 : third route layer

    F3 : 4th route layer

    Shift + F4  : 5th route layer (usually a Power plane)

    F4 :bottom route layer

    Shift + F4 : Part bdocu layer.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • oldmanraskers
    0 oldmanraskers over 10 years ago

    Thank - that really helped me out image