Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) autorouting setup
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 187 subscribers
  • Views 2949 views
  • Users 0 members are here
Related

autorouting setup

e14 Contributor
e14 Contributor over 17 years ago

Hi,

 

Where can I find a tutorial about autorouting configurations ?  I don´t

understand many of parameters in autoroute menu.

 

Cost:

====

Via, NonPref, ChangeDir, OrthStep, DiagStep, ExtdStep, BonusStep, MalusStep,

PadImpact, SmdImpact, BusImpact, Hugging, Polygon

 

Maximum:

========

Via, Segments, ExtdSteps, RipupLevel, RipupSteps, RipupTotal

 

 

How does each of these parameters affect autorouting process ?

 

How are the relationship beetween paramerters ?

 

 

Regards,

 

Leandro

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Your routing grid should be about 5 to 10 times smaller than lead pitch.

    and yes, of course it must include the lead grid or the traces can not

    route!

     

    Clearances in DRC are should be determined by the limits of

    manufacturing processes and are used to make sure the routed board can

    be reliably manufactured, you can set them to whatever limits your board

    house can manufacture. Setting them to get a good routing is wrong.

     

    If you want less vias, you can try increasing the "cost" of vias

    relative to other entities. The router evaluates which routing is best

    by minimizing the "cost" of the entire board, so if you make vias 10x

    more costly, it will make eliminating them 10x more important in the

    routing process. This will also make routing 10x more difficult for the

    computer and perhaps take 10x or even 100x longer.

     

    If you have critical trace alignments, like a hi speed differential

    pair, I will tell you that the EAGLE autorouter will never be able to

    handle that, do it manually. If you want two traces to be close or far

    away, well some software will do this, not EAGLE, do it manually. if you

    want your board to have nice patterns on it, that usually means more

     

    you should realize that no autorouter produces work comparable to a

    manual routing. the parameters that work for one board will likely not

    work so well on the next one. also the various passes of optimization

    are usually more important than tweaking the values, lowering the via

    count may have a side effect of awkward trace placement for example. the

    object is a good balanced outcome for all parameters.

     

    generally, i would start with power and other critical nets and manually

    route them first. then i would let the autorouter finish the board if it

    is complex.

     

    It is true that EAGLE documentation for the autorouter is weak, but it

    is also true that anything critical is normally handled manually, so

    there is little interest in tweaking the autorouter, mainly people want

    it to get 100% routing. However, if you like to experiment with it and

    you think you have improved parameters, I'm sure some will like to try

    your tweaked parameters on their board, so please share them with us!

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 17 years ago

    I´m really like Eagle software.  I believe that is a great software, very

    easy to use and good enough for almost all problem involving PCB design.

     

    My boards routes 100%.  It´s not my problem.

     

    But I thing that trace alignment, trace distribuition and a reduced numbers

    of vias are important too.  Why I would like to have better controll of

    routing process.

     

    I did several experiments, having routed some PCBs many times, changing some

    parameters.  I realized that some rules are very important to get good

    resoults:

     

    1) Fine-pitch components should be aligned with the grid  (all pads);

     

    2) Routing grid should be (at least) equal the small pitch of fine-ptich

    components.  If the pitch is not a exact routing grid multiple (ex.:

    pitch=0.50mm and routing grid = 0.25mm), we need a very small routing grid

    to route same PCB.

     

    3) DRC clearance should be small than pitch minus trace width (its a

    physic´s problem, space is need for trace gets pad).  At least for the

    clearance beetwen wires should be in according to this roule.

     

     

    This few rules (some of them are obvious) and many others not listed could

    be writen in a small tutorial to help people to get best resoults with

    Eagle, without wasting time.

     

    But, even using roules like those above, I´m sure that we can get more from

    Eagle software.  If there are several paramaters available in routing

    options, why don´t use them in our benefit ?  Why don´t clarify users about

    meaning of this paramenters ?  For example, what does "costs" mean ?

     

     

    Many people use Eagle because software´s qualities.  And I´d like to see

    more and more people using Eagle.

     

    Mainly, I´d like to see Eagle being used in the professional world, without

    any distinction from others called "professionals softwares".  I´m sure

    Eagle software has resources to make this real.  But Eagle people must teach

    us to use all resources of Eagle software cans offer.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    normally they do not need to be changed. if your board will not route it

    is likely due to issues of the placement and routing grids beings too

    coarse.

     

    the parameters indicate the what "cost" each of the routing entities

    uses, the router will try to minimize the total cost of the board. you

    will note that there are many passes with some different emphasis that

    try to give you a nice board. this is characteristic of most "simulated

    annealing" type optimizers, so perhaps EAGLE uses this as its algorithm.

     

    in general, if your board routes 100% or reasonably close to it, you

    would not need to alter the costs. rather spend your precious time

    manually "cleaning up" any awkward results from the autorouter.

     

    most problems i've seen with autorouting are the result of the

    aforementioned grid or layer setup problems.

     

    • Cancel
    • Vote Up 0 Vote Down